I connected the two boards to page 28 of themurata_quick_start_guide_linux.pdf manual.At the same time, I built the new mirror file as described in the following post in the community https://community.nxp.com/thread/496328.
1) According to the above connection I will wfi test pass without problem,but I don't know how bluetooth should be connected to the board in the hardware part.According to table 10 on page 49 of the manual, it is indicated that I should connect GPIO2 and UART5. Where should the specific terminals be connected.
2) The above verification was done on the i.MX6Qsabresd Board.How to extract the patched Murata 1MW WiFi/BT kernel source code from yocto.
Hi,
You will need to connect the Flat Flex Cable that came with the uSD-M.2 adapter. Check this post: https://community.murata.com/s/feed/0D55F000098u6o6SAA , which discusses how to connect the FFC.
In case you need clarifications or have further questions, feel free to contact Murata at their technical support forum: https://community.murata.com/ .
Best regards
I suggest that you enter your question in the Murata Technical Support, they can help you, with your inquiry since the module was directly made for the i.MX6 platform