i.MX6Q with kernel 4.13.0 panic on irq_request

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q with kernel 4.13.0 panic on irq_request

861 Views
romaincrausaz
Contributor I

Dear all,

I updated the source file of my i.MX6Q from kernel 4.4 to kernel 4.13 and since then my driver to handle the communication with our FPGA (connected with the WEIM bus) throws a kernel panic on the irq_request.

On kernel 4.4 everything was working properly.

I attached a part of the device tree and the kernel panic messages.

I am not an expert with device tree definition but the attached definition was working on 4.4

Here is the call to the irq_request function:

    irq = irq_of_parse_and_map(pdev->dev.of_node, 0);

    if(irq == NO_IRQ){
        printk(KERN_ERR "fpga: no irq\n");
        return -ENODEV;
    }
    
    printk(KERN_INFO "fpga: irq = %d\n", irq);

    //ret = request_irq(irq, (void *)irq_read_handler, IRQF_TRIGGER_HIGH, "driver_fpga", (void *)irq_read_handler);
    ret = devm_request_irq(&pdev->dev, irq, (void *)irq_read_handler, IRQF_TRIGGER_HIGH, pdev->name, pdev);
    if(ret < 0){
        printk(KERN_ERR "fpga: irq request failed : %d\n", ret);
        return ret;
    }

I tried both function (request_irq and devm_request_irq) and the result is the same.

Thanks for your help

Best regards

Labels (3)
0 Kudos
3 Replies

647 Views
romaincrausaz
Contributor I

Hi Fabio,

Thanks for your answer. I checked the files however I was not able to put it in my context.

Regards

Romain

0 Kudos

647 Views
igorpadykov
NXP Employee
NXP Employee

Hi Romain

kernel 4.13 is not supported by nxp, one can try with ones described

on i.MX official software page

i.MX Software|NXP 

Best regards
igor

0 Kudos

647 Views
fabio_estevam
NXP Employee
NXP Employee

Hi Romain,

Take a look at this dts file where a FPGA is connected via WEIM:

arch/arm/boot/dts/imx51-ts4800.dts

And then look at its driver implementation:
drivers/irqchip/irq-ts4800.c

Hope this helps.

Regards,

Fabio Estevam

0 Kudos