i.MX6Q with Andriod 5 automatic reboot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q with Andriod 5 automatic reboot issue

765 Views
johntseng
Contributor I

Dear Supporter

Our customize board is similar with the i.MX 6Q sabresd except the DDR, and we have completed the ddr test,  about 70% of the boards will reboot after the Andriod 5 OS running for 24-48 hours, 15% will reboot after 48-72 hours, 5% will reboot after 2 hours.

CPU: MCIMX6Q5EYM10AD

Memory: 512MB+512MB

EMMC: 8GB

Kernel version: 3.10.53
Android OS Version : Android 5.0

The dump log as below:

[16:49:50.550][  133.564597] galcore 130000.gpu: **** DPM device timeout ****

[16:49:50.565][  133.570298] [<807f1b40>] (__schedule+0x350/0x724) from [<807f2104>] (io_schedule+0x68/0x94)

[16:49:50.565][  133.578684] [<807f2104>] (io_schedule+0x68/0x94) from [<800a501c>] (sleep_on_page+0x8/0x10)

[16:49:50.581][  133.587064] [<800a501c>] (sleep_on_page+0x8/0x10) from [<807f04c8>] (__wait_on_bit_lock+0x6c/0xb8)

[16:49:50.581][  133.596045] [<807f04c8>] (__wait_on_bit_lock+0x6c/0xb8) from [<800a500c>] (__lock_page+0x94/0x9c)

[16:49:50.597][  133.604933] [<800a500c>] (__lock_page+0x94/0x9c) from [<800dc21c>] (migrate_pages+0x4b4/0x4cc)

We have tried to reduce the IMX6 processor frequency and increase the  CPU voltage, the board will running fine.

Would you give me some advice to analyse this issue? Thanks.

 

Labels (2)
0 Kudos
2 Replies

555 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

one can check if i.MX Android™ KK4.4.3_2.0.1 patches are included

as described in attached document and that gpu has sufficient memory with below hints:

Memory Management on i.MX6 Android 

Test without gpu usage (with minimal image) to see if this is caused by power supplies ripples,

check power requirements given in Table 2-6. Power and decouple recommendations

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

555 Views
johntseng
Contributor I

Thanks Igor, we'll test again after updated the new patchs.

0 Kudos