i.MX6Q in secure state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q in secure state

1,222 Views
scribnote5
Contributor I

Hi, expert.

My platform has a Cortex-A9(Sabre Lite, i.mx6q), It supports the trustzone tech.

I have a question about the secure state.

I read questions and answers about secure state in https://community.nxp.com/thread/394659https://community.nxp.com/thread/394176.

Following prior questions and answers, sabre lite boots Linux in the secure state. 

So Linux completely boots in the secure world and runs the applications in the secure world without any state change.

Are these right? 

Best, Wishes 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,132 Views
art
NXP Employee
NXP Employee

With the specially configured kernel, e.g. as the kernel configuration by Boundary Devices, Linux completely boots and runs in the secure world without any state change.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply