i.MX6Q controller that is placed in CPU2 is Rev1 (or Rev1.3)…?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Q controller that is placed in CPU2 is Rev1 (or Rev1.3)…?

1,089 次查看
mithunpsappanna
Contributor I

Hi,

Please help to know MCIMX6QAICPU2 daughter card has i.MX6Q controller that is placed in CPU2 is Rev1 (or Rev1.3)…?

Thanks & Regards

mithun@

0 项奖励
回复
2 回复数

998 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Mithun,

We are using the MCIMX6Q6AVT10AC  the letter C it is the value for the version so it is REV 1.2


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

998 次查看
mithunpsappanna
Contributor I

Dear Jaime.

Thanks & Regards

Mitun P S

Mob: +91 7899111606

Dir: +91 080- 40604201

www.em.avnetasia.com<http://www.em.avnetasia.com/>;

0 项奖励
回复