i.MX6Q - audio output (Text to Voice)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Q - audio output (Text to Voice)

1,600 次查看
Sangraemelb
Contributor II

Hi! I am working on i.MX6Q for Text to Audio.

 

The audio outputs are just to transfer audio input to the outputs.

 

I would like to generate the audio signal like below or any other way.

It doesn't have to be PWM signal outputs.

It reads a data and generate audio signals, not regenerate audio signals.

 

 

Sangraemelb_0-1637284682869.png

 

Regards,

Sangrae

 

 

0 项奖励
回复
4 回复数

1,583 次查看
Sangraemelb
Contributor II

Hi! 

Thank you for the info.

 

Is there any reference design?

 

It is hard to find information about MQS.

 

Regards,

Sangrae

 

0 项奖励
回复

1,571 次查看
b36401
NXP Employee
NXP Employee

We have no example for i.MX6. Sorry for the inconvenience.

0 项奖励
回复

1,596 次查看
b36401
NXP Employee
NXP Employee

i.MX6 MQS is used to generate medium quality audio via standard GPIO and produces PWM signal, fixed in amplitude and frequency, but varying in duty cycle. So additional an RC filter is needed at output, this will produce medium quality sound without an additional DAC.

0 项奖励
回复

1,577 次查看
Sangraemelb
Contributor II

Hi! 

 

Does that mean all GPIO can be configured as MQS_LEFT or MQS_RIGHT pin?

Or just PWM1 and PWM2 which can also be configured as GPIO?

 

Can I get more information about MQS?

It is really hard to find.

 

 

Sangraemelb_0-1637295651902.png

From i.MX 6Dual/6Quad Applications Processor Reference Manual / page 153

 

Regards,

Sangrae

 

 

0 项奖励
回复