i.MX6Q and I.MX6DL./unused RTC_XTALI, RTC_XTALO(use spi NOR boot.)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6Q and I.MX6DL./unused RTC_XTALI, RTC_XTALO(use spi NOR boot.)

跳至解决方案
1,315 次查看
soichiyamamoto
Contributor V

HI,

I use i.MX6Q and I.MX6DL.

and ,I use spi NOR boot.

(I Know In addition, I know ERR007926.)

but I do not use  RTC_XTALI, RTC_XTALO.

Please tell me the unused handling of RTC_XTALI, RTC_XTALO.

Best regards,

soichi

标签 (2)
1 解答
1,087 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

if 32.768 kHz external crystal oscillator is not used

RTC_XTALI can be tied to ground, RTC_XTALO left unconnected.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,088 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soichi

if 32.768 kHz external crystal oscillator is not used

RTC_XTALI can be tied to ground, RTC_XTALO left unconnected.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------