i.MX6Q V4L2 IOCT- IPU_ROTATE_HORIZ_FLIP can't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q V4L2 IOCT- IPU_ROTATE_HORIZ_FLIP can't work

Jump to solution
1,481 Views
xiaoqianlin
NXP Employee
NXP Employee

Hi,

Cloudtech reported i.MX6Q V4L2 IOCT- IPU_ROTATE_HORIZ_FLIP  can't work. Can you help to check?

imx6q  android 4.2.2平台上用adv7180  camera 由于拍照方向水平镜像了需要用到ipu 来实现 H mirror, 通过
V4L2  IOCTL
调用但目前case V4L2_CID_MXC_ROT:中的IPU_ROTATE_HORIZ_FLIP 不起作用,但IPU_ROTATE_VERT_FLIP这个垂直镜像可以。

Linda Lin
1 Solution
1,196 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Hi Linda, for IPU display channel, it can only support IPU_ROTATE_VERT_FLIP(vertical filp), for other kind of rotation, the customer should use IPU task to implement it.

View solution in original post

3 Replies
1,197 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Hi Linda, for IPU display channel, it can only support IPU_ROTATE_VERT_FLIP(vertical filp), for other kind of rotation, the customer should use IPU task to implement it.

1,196 Views
gusarambula
NXP TechSupport
NXP TechSupport

Thank you, Quiang Li!

0 Kudos
Reply
1,196 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Only one FLIP can work at the same time, so IPU_ROTATE_HORIZ_FLIP + IPU_ROTATE_VERT_FLIP can't work.

0 Kudos
Reply