Hi All,
I was running some PCIe tests on SabreSD board. The 4 CPU cores and the PCI worked fine. When I changed the PCIe card the PCI link stopped working. When I started debugging the problem I found that Core 2 and Core 3 are not working! only core0 and core1 are running:
root@imx6qsabresd:~# cat /proc/cpuinfo
processor : 0
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : swp half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10
processor : 1
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : swp half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10
Hardware : Freescale i.MX6 Quad/DualLite (Device Tree)
Revision : 0000
Serial : 0000000000000000
The output of bare-metal SDK also shows that only Core0 and Core1 are running:
Select test to run:
mc
Running the GIC Multicore Test
Starting and sending SGIs to secondary CPUs for "hello world"
secondary main cpu: 1
Is there any chip registers that I can check to get more information about the cores and enable the 2 disabled cores?
I still can run Linux, network, ssh , uart console, ...etc Is it possible that the i.MX6 Chip was damaged?
Thanks,
Tarek
解決済! 解決策の投稿を見る。
Hi Yuri,
I think I found the problem. I have accidentally written to Core2&3 power gating OTP register.
root@imx6qsabresd:/unit_tests# ./memtool -32 0x021BC4D0 1
E
Reading 0x1 count starting at address 0x021BC4D0
0x021BC4D0: 80000000
Now the 2 cores gone forever ......:smileysad:
Hello,
Please check if VDD_ARM23_IN is proper.
Also, You may use the example in attachment of the following thread
to check multi-core operations.
Integrating Processor Expert for i.MX and ARM GCC with Eclipse
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
I think I found the problem. I have accidentally written to Core2&3 power gating OTP register.
root@imx6qsabresd:/unit_tests# ./memtool -32 0x021BC4D0 1
E
Reading 0x1 count starting at address 0x021BC4D0
0x021BC4D0: 80000000
Now the 2 cores gone forever ......:smileysad:
:-)