i.MX6Q SSI with zl38063

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q SSI with zl38063

1,192 Views
kaneshi
Contributor I

we used an echo cancellation chip(zl38063) as the sound card for  our i.MX6Q customer board.We are referring to the i.MX6ULL scheme, but this chip uses the SAI interface in i.MX6ULL.

the folowing is imx6ull device tree configuration

zl380-codec {
compatible = "ms,zl38040", "ms,zl38050", "ms,zl38060", "ms,zl38080";
status = "okay";
};

sound {
compatible = "microsemi,microsemi-dac";
i2s-controller = <&sai2>;

};

because i.MX6Q does't have a SAI interface,so i changed the SAI to SSI. 

can SSI replace the SAI interface?

Labels (4)
0 Kudos
4 Replies

976 Views
cilymo
Contributor I

Hi, Kane:

     Did your zl38063 driver porting OK? Can share your driver (codec and machine) to me? 

Thanks !

And my email address is cily.mo@d-3.com.hk

0 Kudos

976 Views
kaneshi
Contributor I

Hi cilymo

the driver code need to mask HBI function.

yunzhong1912@163.com

0 Kudos

976 Views
cilymo
Contributor I

Thank you very much.

0 Kudos

976 Views
igorpadykov
NXP Employee
NXP Employee

Hi kane

i.MX6Q SSI interface is supported in nxp bsps, one can check

software for i.MX6Q Sabre SD board and build images for that board using

linux documentation Linux L4.14.78_1.0.0 Documentation

WM8962 codec is supported and described in Chapter 7 Audio attached Linux Manual.

linux/arch/arm/boot/dts/imx6qdl-sabresd.dtsi

imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Example of connections i.MX6Q SSI with codec

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
SABRE Platform for Smart Devices | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos