i.MX6Q-SDB board bringup with Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q-SDB board bringup with Linux

ソリューションへジャンプ
9,063件の閲覧回数
sergeykras
Contributor I

Recently we bought the i.MX6Q-SDB board and I need to jump quickly to the application development. The board was supplied with bootable  SD card with Android. I want to keep this SD and prepare another one based on Linux. After several hours of researching and studding many pdf documents I was frustrated that I don't see simple instruction how prepare such SD. So my questions are:

1) I see 2 possible BSP to work with: fsl-yocto-3.10.17_1.0.0 or L3.0.35_4.1.0. Which one is more suitable for rapid development?

2) Do I need to compile uImage & rootfs, or may I use the created binaries from L3.0.35_4.1.0_130816_images_MX6?

   * I prefer to work on Windows + Cygwin

3) Can I boot the Linux image directly via TFTP loading from original "MX6Q SABRESD U-Boot >"?

4) I need the simple instruction how to burn uBoot + Linux from L3.0.35_4.1.0_130816_images_MX6 to new SD card.

Thanks in advance.

Sergey

タグ(1)
0 件の賞賛
返信
1 解決策
4,234件の閲覧回数
Yuri
NXP Employee
NXP Employee

I manged to get Linux image working, using the next :

$ sudo dd if=u-boot-imx6qsabresd_sd.imx of=/dev/sdb bs=512 seek=2 conv=fsync

$ sudo dd if=uImage_imx_v7_defconfig of=/dev/sdb bs=512 seek=2048 conv=fsync

$ sudo dd if=uImage-imx6q-sabresd.dtb of=/dev/sdb bs=512 seek=20480 conv=fsync

$ sudo fdisk /dev/sdb

The following are parameters for fdisk (each followed by <ENTER>):

u [switch the unit to sectors instead of cylinders]

d [repeat this until no partition is reported by the 'p' command ]

n [create a new partition]

p [create a primary partition]

1 [the first partition]

+20M [20MB,  enough space for thekernel, the boot loader and its configuration data]

<enter> [using the default value will create a partition that spans to the last sector

of the medium]

w [ this writes the partition table to the medium and fdisk exits]

$ sudo mkfs.ext3 /dev/sdb1

$ mkdir /home/user/mountpoint

$ sudo mount /dev/sdb1 /home/user/mountpoint

$ sudo mount -o loop -t ext3 fsl-image-weston-imx6qdlsolo.ext3 /home/user/rootfs

$ cd /home/user/rootfs

$ sudo cp -a * /home/user/mountpoint

$ sudo umount /home/user/mountpoint

$ sudo umount /home/user/rootfs

Under U-boot after SD boot.

U-boot> setenv loadaddr 0x12000000

U-boot> setenv loadaddr 0x12000000

U-boot> setenv fdt_high 0xffffffff

U-boot> setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'

U-boot> setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666'

U-boot> setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x3000;mmc read ${fdt_addr} 0x5000 0x800;bootm ${loadaddr} - ${fdt_addr}'

U-boot> setenv bootcmd 'run bootcmd_mmc'

Reset ....

元の投稿で解決策を見る

0 件の賞賛
返信
14 返答(返信)
4,233件の閲覧回数
sergeykras
Contributor I

Upon succeeding to load the Linux from SD card I need to run one of GStreamer tests. The suggested fsl-image-weston-imx6qdlsolo.ext3 contains GStreamer tools but, unfortunately, it doesn't contain gst-fsl-plugins (neither mfw_v4lsrc nor vpuenc).
Is it possible to download from somewhere the gst-fsl-plugins binaries?  Or I need to compile it by myself? What is the correct place of binaries/sources to download in case I have fsl-yocto-3.10.17_1.0.0 kernel?

0 件の賞賛
返信
4,233件の閲覧回数
sergeykras
Contributor I

Hi,

I did exactly as it was explained. Have used dd tool on Linux PC to burn these 2 files:

u-boot-imx6qsabresd_sd.imx

uImage_imx_v7_defconfig

But when butting u-boot stops at the following lines:

------------------------------------------------

mmc1 is current device

** Unrecognized filesystem type **

** Unrecognized filesystem type **

Booting from net ...

BOOTP broadcast 1

BOOTP broadcast 2

BOOTP broadcast 3

BOOTP broadcast 4

BOOTP broadcast 5

Retry count exceeded; starting again

------------------------------------------------

Where have I mistaken?

0 件の賞賛
返信
4,233件の閲覧回数
Yuri
NXP Employee
NXP Employee

  It is needed to stop U-boot (just after initial boot) and configure U-boot
environment for required boot options. Please take a look at section 8.2
(Run the Image from MMC/SD) of "i.MX_6_SABRE-SD_Linux_User's_Guide.pdf"
[Yocto docs].

Have a great day,
Yuri

--------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
--------------------------------------------------------------------------------------------

4,234件の閲覧回数
sergeykras
Contributor I

Thanks, I already found this section 8.2, but after doing it I encountered a problem discussed here: https://community.freescale.com/thread/324033 (Bad Data CRC before kernel starts). I changed ${loadaddr} 0x800 0x2000 -> ${loadaddr} 0x800 0x3000 as it was suggested. And the kernel started to boot!!! But the second described problem of mmcblk0p2 / mmcblk0p1 still present. Changing it from 02 to 01 doesn't help:

...

input: gpio-keys.27 as /devices/soc0/gpio-keys.27/input/input6

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:33:38 UTC (2018)

ALSA device list:

  #0: wm8962-audio

  #1: imx-hdmi-soc

VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2): error -6

Please append a correct "root=" boot option; here are the available partitions:

1f00 32 mtdblock0  (driver?)

b300 1931264 mmcblk0  driver: mmcblk

b308 7757824 mmcblk1  driver: mmcblk

b320 128 mmcblk1rpmb  (driver?)

b318 2048 mmcblk1boot1  (driver?)

b310 2048 mmcblk1boot0  (driver?)

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2kernel)

Please help!!

0 件の賞賛
返信
4,234件の閲覧回数
Yuri
NXP Employee
NXP Employee

Let me look at U-boot environment (U-boot command "pri")

0 件の賞賛
返信
4,234件の閲覧回数
sergeykras
Contributor I

U-Boot > pri

baudrate=115200

boot_fdt=try

bootargs_base=setenv bootargs console=ttymxc0,115200

bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p2 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24

bootcmd=run bootcmd_mmc

bootcmd_mfg=run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x3000;mmc read ${fdt_addr} 0x5000 0x800;bootm ${loadaddr} - ${fdt_addr}

bootdelay=1

bootscript=echo Running bootscript from mmc ...; source

console=ttymxc0

ethact=FEC

ethaddr=00:04:9f:02:df:d2

ethprime=FEC

fdt_addr=0x18000000

fdt_file=imx6q-sabresd.dtb

fdt_high=0xffffffff

initrd_addr=0x12C00000

initrd_high=0xffffffff

ip_dyn=yes

loadaddr=0x12000000

loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};

loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}

loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}

mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off

mmcargs=setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot}

mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;

mmcdev=1

mmcpart=1

mmcroot=/dev/mmcblk0p2 rootwait rw

netargs=setenv bootargs console=${console},${baudrate} ${smp} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp

netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;

script=boot.scr

uimage=uImage

Environment size: 2211/8188 bytes

0 件の賞賛
返信
4,234件の閲覧回数
Yuri
NXP Employee
NXP Employee

Also, the most simple way :

$ sudo dd if=fsl-image-gui-imx6qsabresd.sdcard of=/dev/sdb bs=1M

Task #4 - Deploy and test

0 件の賞賛
返信
4,234件の閲覧回数
sergeykras
Contributor I

Where the fsl-image-gui-imx6qsabresd.sdcard file may be found? I have only fsl-image-x11-imx6qdlsolo.sdcard (from L3.10.17_1.0.0_ga_140404_images_MX6.tar.gz)

0 件の賞賛
返信
4,234件の閲覧回数
Yuri
NXP Employee
NXP Employee

The file "fsl-image-gui-imx6qsabresd.sdcard" has been mentioned just as an example.
~Yuri.

0 件の賞賛
返信
4,235件の閲覧回数
Yuri
NXP Employee
NXP Employee

I manged to get Linux image working, using the next :

$ sudo dd if=u-boot-imx6qsabresd_sd.imx of=/dev/sdb bs=512 seek=2 conv=fsync

$ sudo dd if=uImage_imx_v7_defconfig of=/dev/sdb bs=512 seek=2048 conv=fsync

$ sudo dd if=uImage-imx6q-sabresd.dtb of=/dev/sdb bs=512 seek=20480 conv=fsync

$ sudo fdisk /dev/sdb

The following are parameters for fdisk (each followed by <ENTER>):

u [switch the unit to sectors instead of cylinders]

d [repeat this until no partition is reported by the 'p' command ]

n [create a new partition]

p [create a primary partition]

1 [the first partition]

+20M [20MB,  enough space for thekernel, the boot loader and its configuration data]

<enter> [using the default value will create a partition that spans to the last sector

of the medium]

w [ this writes the partition table to the medium and fdisk exits]

$ sudo mkfs.ext3 /dev/sdb1

$ mkdir /home/user/mountpoint

$ sudo mount /dev/sdb1 /home/user/mountpoint

$ sudo mount -o loop -t ext3 fsl-image-weston-imx6qdlsolo.ext3 /home/user/rootfs

$ cd /home/user/rootfs

$ sudo cp -a * /home/user/mountpoint

$ sudo umount /home/user/mountpoint

$ sudo umount /home/user/rootfs

Under U-boot after SD boot.

U-boot> setenv loadaddr 0x12000000

U-boot> setenv loadaddr 0x12000000

U-boot> setenv fdt_high 0xffffffff

U-boot> setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'

U-boot> setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666'

U-boot> setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x3000;mmc read ${fdt_addr} 0x5000 0x800;bootm ${loadaddr} - ${fdt_addr}'

U-boot> setenv bootcmd 'run bootcmd_mmc'

Reset ....

0 件の賞賛
返信
4,234件の閲覧回数
sergeykras
Contributor I

Yuri, many thanks! Now it works. I do not know where it was my mistake, but now it is loading. May be the problem was in fsl-image-fb-imx6qdlsolo.ext3 image, now I have used suggested fsl-image-weston-imx6qdlsolo.ext3

0 件の賞賛
返信
4,234件の閲覧回数
Yuri
NXP Employee
NXP Employee

Strictly speaking neither Yocto nor LTIB packages are not intended for development.
They are intended for different configuration building. Nevertheless it is possible
to get kernel sources and configure, say, Eclipse configuration for applications design
for both approaches. It makes sense to use Yocto, since LTIB will not used more for
new releases. 

   As for boot SD preparing, please refer to section 7 (Using a Linux Host to Set Up
an SD/MMC Card) of of “i.MX_6_SABRE-SD_Linux_User's_Guide.pdf” in
fsl-yocto-3.10.17_1.0.0 documentation. Of course You may use kernel, U-boot and rootFS
from demo images.

     TFTP may be used, as shown in section 6 (Download Images by Bootloader or NFS).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,234件の閲覧回数
sergeykras
Contributor I

Yuri, thanks for your explanation. But still wonder is it possible to use cfimager (cfimager-imx.exe) on Windows to burn bootable SD containing uBoot with Linux?

0 件の賞賛
返信
4,234件の閲覧回数
Yuri
NXP Employee
NXP Employee

cfimager was not tested with i.MX6

0 件の賞賛
返信