Hello,
We using Atheros ath9k AR9462/AR9482 PCI-e module in our's i.MX6Q custom board.
I downloaded a compat-drivers-3.9-rc1-3 from Linux-Wireless, and generate ath9k driver modules.
These modules are loaded sequentially by:
compat.ko
cfg80211.ko
mac80211.ko
ath.ko
ath9k_hw.ko
ath9k_common.ko
ath9k.ko
Then download libnl and iw tools scan and connected to WIFI AP.
I can find and ping WIFI AP but the browser can not connect to the network.
Does this mean that ath9k driver modules have been ready?
About the ath9k HAL and frameworks without any reference resources.
How to modify android wifi HAL and frameworks?
init.rc also need to modify it?
Thank you for anyone that will give us some hints.
Hi, Peter
I also want to apply ar9462 pcie module to our's i.MX6Q custom board in android 4.2.2 platform.
Have you solve this problem later?
Would you please give me any suggestion ?
Thank you a lot.
Leo
Hi, Leo
The method posted by byungchul should work.
I can bring up WLAN by system UI with compat-wireless driver by similar way.
As for the HAL and private lib for wpa_supplicant, you can refer to the source code of Android-x86.
However, I still have some problems on suspend/resume. I am not sure if this results from the difference of kernel version or not because we use v3.4
Good luck.
Hi, peter.
This a my build methods.
I hope this tips will help you.
0. Kernel configuration
CONFIG_WIRELESS_EXT=y
CONFIG_NET_SCHED=y
CONFIG_CFG80211=m
CONFIG_CFG80211_WEXT=y
CONFIG_WIRELESS_EXT_SYSFS=y
CONFIG_LIB80211=y
CONFIG_MAC80211=m
CONFIG_ATH_COMMON=m
CONFIG_ATH9K_HW=m
CONFIG_ATH9K_COMMON=m
CONFIG_ATH9K=m
CONFIG_ATH9K_PCI=y
CONFIG_ATH9K_RATE_CONTROL=y
1. select drivers (compat-wireless-3.6.8-1)
./scripts/driver-select ath9k
2. comile driver
make ARCH=arm CROSS_COMPILE=arm-linux- KLIB=/opt/mx6/linux-3.0.35 KLIB_BUILD=/opt/mx6/linux-3.0.35
3. install modules
sudo ./install.sh
4. connection test
1) WEP128, ASCII key
ifconfig wlan0 up
iwconfig wlan0 essid "SoftAP-E1" key s:0123456789012
2) WAP/WPA2
You need to edit the /etc/wpa_supplicant.conf file as described in WPA_Supplicant and according to what you got from #Access point discovery. Then, issue this command:
wpa_supplicant -i wlan0 -B -c /etc/wpa_supplicant.conf
or
wpa_supplicant -i wlan0 -c /etc/wpa_supplicant.conf &
</etc/wpa_supplicant.conf>
ctrl_interface=/var/run/wpa_supplicant
network={
ssid="SoftAP-E0"
psk="1234567890"
key_mgmt=WPA-PSK
proto=WPA2
pairwise=CCMP
group=CCMP
}
3) ping test
route add default gw 192.168.0.1
ping ftp.kernel.org
4) speed test
<client>
iperf -c 10.11.12.232
<server>
iperf -s
<install.sh>
#!/bin/sh
MODPATH=/opt/mx6/rootfs/lib/modules/3.0.35-2310-gc27cb38/kernel
MODROOT=/opt/mx6/rootfs/lib/modules
cp -vrf ../net/rfkill/rfkill-regulator.ko $MODPATH/net/rfkill/rfkill-regulator.ko
cp -vrf ./net/mac80211/mac80211.ko $MODPATH/net/mac80211/
cp -vrf ./net/wireless/cfg80211.ko $MODPATH/net/wireless/
cp -vrf ./drivers/net/wireless/ath/ath.ko $MODPATH/drivers/net/wireless/ath/
cp -vrf ./drivers/net/wireless/ath/ath9k/ath9k.ko $MODPATH/drivers/net/wireless/ath/ath9k/
cp -vrf ./drivers/net/wireless/ath/ath9k/ath9k_htc.ko $MODPATH/drivers/net/wireless/ath/ath9k/
cp -vrf ./drivers/net/wireless/ath/ath9k/ath9k_hw.ko $MODPATH/drivers/net/wireless/ath/ath9k/
cp -vrf ./drivers/net/wireless/ath/ath9k/ath9k_common.ko $MODPATH/drivers/net/wireless/ath/ath9k/
mkdir -p $MODROOT/compat
cp -vrf ./compat/sch_fq_codel.ko $MODROOT/compat/
cp -vrf ./compat/sch_codel.ko $MODROOT/compat/
cp -vrf ./compat/compat.ko $MODROOT/compat/