i.MX6Q MMDCx_MDASP[CS0_END] for 4GB with 2CS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q MMDCx_MDASP[CS0_END] for 4GB with 2CS

Jump to solution
912 Views
m_c
Senior Contributor I

We found two different values by below three methods for CS0_END for 4GB with 2CS. Why difference value? Which is right?

1. Page 3840 of IMX6DQRM revision 2 is 0x3f

pastedImage_1.png

2. Page 3926 of IMX6DQRM revision 2 is 0x47.

2048M/32M+0x7=0x40+0x7=0x47

pastedImage_5.png

3. Mx6DQSDL DDR3 Script Aid V0.09.xlsx is 0x47

pastedImage_4.png

pastedImage_7.png

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
729 Views
Yuri
NXP Employee
NXP Employee

  The case MDASP[CS0_END] = 0x3F means :

CS0 is responsible for address range 0x1000_0000 - (0x8000_0000 - 1)

CS1 is responsible for address range 0x8000_0000 - (0xFFFF_FFFF)

  The case MDASP[CS0_END] = 0x47 means :

CS0 is responsible for address range 0x1000_0000 - (0x9000_0000 - 1)

CS1 is responsible for address range 0x9000_0000 - 0xFFFF_FFFF


Basically both may be used.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
730 Views
Yuri
NXP Employee
NXP Employee

  The case MDASP[CS0_END] = 0x3F means :

CS0 is responsible for address range 0x1000_0000 - (0x8000_0000 - 1)

CS1 is responsible for address range 0x8000_0000 - (0xFFFF_FFFF)

  The case MDASP[CS0_END] = 0x47 means :

CS0 is responsible for address range 0x1000_0000 - (0x9000_0000 - 1)

CS1 is responsible for address range 0x9000_0000 - 0xFFFF_FFFF


Basically both may be used.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply