Hello Champs,
I have little trouble of capturing in IPU at certain resolutions.
Let me check, is there any restrictions in resolution or proportions other than written in RM page 458.
"Frame size: up to 8192 x 4096 pixels (including blanking intervals)"
BR,
N.S.
Hi Nori
you are right :Frame size: up to 8192 x 4096 pixels
as described i.MX6DQ Reference Manual p.2723
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
There are no other restrictions in max. resolution
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------