Hello,
I'm trying to play mp4 on GStreamer and VPU of i.MX6Q. And I want to use qtdemux and isink, but an error occurs.
How can I play using qtdemux and isink?
My operation is below:
gst-launch filesrc location=/mnt/floppy/1sec_10frame.mp4 ! 'video/quicktime' ! qtdemux ! queue ! vpudec ! mfw_isink
It's no problem when using aiurdemux.
gst-launch filesrc location=/mnt/floppy/1sec_10frame.mp4 ! 'video/quicktime' ! aiurdemux ! queue ! vpudec ! mfw_isink
filesrc: 0.10.35
aiurdemux: 3.0.5
vpudec: 3.0.5
qtdemux: 0.10.30
The error occurs in vpu_DecGetInitialInfo() of vpu_lib.c.
=====
{
:
BitIssueCommand(pCodecInst, SEQ_INIT);
while (VpuReadReg(BIT_BUSY_FLAG)) ;
val = VpuReadReg(RET_DEC_SEQ_SUCCESS);
if (cpu_is_mx6x()) {
#ifdef MEM_PROTECT
if (val & (1 << 31)) {
:
}
#endif
-> if (pDecInfo->openParam.bitstreamMode && (val & (1 << 4))) {
-> UnlockVpu(vpu_semap);
-> return RETCODE_FAILURE;
}
}
=====
Best Regards,
Daisuke
解決済! 解決策の投稿を見る。
/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:sink: caps = video/x-h264, stream-format=(string)avc, alignment=(string)au, level=(string)2, profile=(string)baseline,
codec_data=(buffer)0142e00dffe100162742e00da918283f600d418041adb7a02f01e97bdf0101000428ce0988,
width=(int)320, height=(int)240, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1
In the case of aiurdemux
codec_data=(buffer)000000012742e00da918283f600d418041adb7a02f01e97bdf01 0000000128ce0988
In the case of qtdemux
codec_data=(buffer)0142e00dffe100162742e00da918283f600d418041adb7a02f01e97bdf0101000428ce0988
I don't know why this happens, so I just modified qtdemux to make it output the "codec_data" of aiurdemux above regardless of the read mp4 file on trial.
The two modification above solved the problem.
I mean I could play a specific mp4 file using qtdemux + vpudec.(non-aiurdemux)
(I cannot play other mp4 file because qtdemux decide "codec_data" statically on trial)
I guess "codec_data" is avcC Data which is in mp4 file.
In the case of qtdemux, "codec_data" equalls avcC, but in the case of aiurdemux, it's little bit modified.
According to the aiurdemux element source code, "codec_data" is decided by FslParserGetDecSpecificInfo() which is fsl parser API.
Could anyone advice me the way to convert "codec_data" of qtdemux to aiurdemux so that qtdemux can decide "codec_data" same as the aiurdemux and play any mp4 files?
Kuniaki
As recommended by DaianeAngolini, have you tried any FFMPEG demuxer?
/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:sink: caps = video/x-h264, stream-format=(string)avc, alignment=(string)au, level=(string)2, profile=(string)baseline,
codec_data=(buffer)0142e00dffe100162742e00da918283f600d418041adb7a02f01e97bdf0101000428ce0988,
width=(int)320, height=(int)240, framerate=(fraction)30/1, pixel-aspect-ratio=(fraction)1/1
In the case of aiurdemux
codec_data=(buffer)000000012742e00da918283f600d418041adb7a02f01e97bdf01 0000000128ce0988
In the case of qtdemux
codec_data=(buffer)0142e00dffe100162742e00da918283f600d418041adb7a02f01e97bdf0101000428ce0988
I don't know why this happens, so I just modified qtdemux to make it output the "codec_data" of aiurdemux above regardless of the read mp4 file on trial.
The two modification above solved the problem.
I mean I could play a specific mp4 file using qtdemux + vpudec.(non-aiurdemux)
(I cannot play other mp4 file because qtdemux decide "codec_data" statically on trial)
I guess "codec_data" is avcC Data which is in mp4 file.
In the case of qtdemux, "codec_data" equalls avcC, but in the case of aiurdemux, it's little bit modified.
According to the aiurdemux element source code, "codec_data" is decided by FslParserGetDecSpecificInfo() which is fsl parser API.
Could anyone advice me the way to convert "codec_data" of qtdemux to aiurdemux so that qtdemux can decide "codec_data" same as the aiurdemux and play any mp4 files?
Kuniaki
Please put all your codes changes into a patch, so it can be easily applied by other (of course, once you solve the codec_data issue). BTW, How codec_data is extracted on a ffmpeg demuxer? that would be interesting to check.
Leo
shigenobukatagiri-b39676, did you find the reason of this problem?
Leo
Hi Tuchiya-san, Leo,
According to my test, it seems qtdemux doesn’t generate complete H.264 ES.
When I use aiurdemux, there are many “00 00 01” start code prefix of NAL in the demuxed H.264 ES file, VPU and VLC (works on PC) can play back.
However in case of qtdemux, demuxed data has few “00 00 01” start code prefix words, neither VPU nor VLC play back
You may see same result by comparing files generated by following command lines.
$ gst-launch -v filesrc location=<file.mp4> ! 'video/quicktime' ! aiurdemux name=demux ! filesink location=raw_aiur.h264
$ gst-launch -v filesrc location=<file.mp4> ! 'video/quicktime' ! qtdemux name=demux ! filesink location=raw_qt.h264
I found a similar discussion as follows. qtdemux may not be the solution to demux H.264 container.
http://gstreamer-devel.966125.n4.nabble.com/QT-Demux-with-strange-ouput-ES-data-td970679.html
Leo,
Could you please give us your comments?
Best Regards,
Shigenobu
Hi,
Let me investigate further but for the moment, lets force the playback to use another demuxer. Move the plugin/element /usr/lib/gstreamer-0.10/libmfw_gst_aiur_demux.so to your $HOME, then run the following pipeline with playbin2:
gst-launch playbi2 uri=file://<media full path> --gst-debug=GST_ELEMENT_FACTORY:3
Check the log.Which demuxer did playbin2 use? Customer may use that one instead of qtdemux.
Leo
Hi Leo,
Thank you for your help.
I tried your test which removing aiurdemux,
playbin2 looks for aiurdemux first.
-> if aiurdemux is not found, qtdemux is the next target. -> playbin2_1.log
-> if qtdemux is not found either, playbin2 outputs error. -> playbin2_2.log
I've confirmed it by removing libgstisomp4.so.
Best Regards,
Shigenobu
jackmao / DaianeAngolini, I need help on this one :smileyhappy:
Leo
Sorry, what´s the problem here?
I see there is a discussion regarding using qtdemux or airdemux, but, I lost the goal of this discussion.
LeonardoSandovalGonzalez, What´s the goal?
Hi Daiane.
Customer must use a non-aiurdemux element, so qtdemux may be an option. However, when using qtdemux, they got errors and playback is not possible. For some reason, the vpudec does not like what is coming from qtdemux, some missing headers as mentioned in previous post:
Re: i.MX6Q: How to play mp4 using VPU and qtdemux
Leo
oh, I got it.
So aiurdemux is not a option. The question is which other mainline demuxer is suitable for the customer´s usecase.
I only know ffmpeg plugins for gstreamer, but I´m not sure how easy would be for including it on the rootfs and if it would be an option.