i.MX6Q: How to increase the VPU frequency?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q: How to increase the VPU frequency?

Jump to solution
10,112 Views
Tarek
Senior Contributor I

Hi,

The VPU clock is currently running at (266MHz) but it should be capable of running at (352MHz).

I understand that this is been tested at Freescale labs but I'm not sure about how successful is that.

I would like to test it myself but I couldn't modify it in Linux drivers.

This is what I've done in mxc_vpu.c:

{
int rate = 352000000;
printk(KERN_ERR "TSE: VPU Parent CLK rate = %d Hz\n",clk_get_rate(vpu_clk->parent));
rate = clk_round_rate(vpu_clk->parent,352000000);
printk(KERN_ERR "TSE: set the VPU Parent CLK %d Hz err = %d\n",rate,clk_set_rate(vpu_clk->parent,rate));
rate = clk_round_rate(vpu_clk,352000000);
printk(KERN_ERR "TSE: set the VPU CLK %d Hz err = %d\n",rate,clk_set_rate(vpu_clk,rate));
printk(KERN_ERR "TSE: VPU CLK rate = %d Hz\n",clk_get_rate(vpu_clk));
}

The frequency jumps to (528MHz) and the VPU doesn't work.

Please provide the source code for change the Clock rate.

Thanks 

Labels (3)
1 Solution
3,957 Views
AnsonHuang
NXP Employee
NXP Employee

Hi,

     Our BSP release has supported VPU running @352MHz, you just need to enable the config in menuconfig:

     CONFIG_MX6_VPU_352M.

View solution in original post

15 Replies
3,958 Views
AnsonHuang
NXP Employee
NXP Employee

Hi,

     Our BSP release has supported VPU running @352MHz, you just need to enable the config in menuconfig:

     CONFIG_MX6_VPU_352M.

3,957 Views
rickchen
Contributor I

Hi Yongcai,

When I tracing the CONFIG_MX6_VPU_352M definition,

I found a code piece that seems lower down the rate of emi_clk and I am wondering why we do this?

in carch/arm/mach-mx6/clock.c:

#ifdef CONFIG_MX6_VPU_352M

    clk_set_rate(&emi_clk, 176000000);

#else

    clk_set_rate(&emi_clk, 198000000);

#endif

Thanks

0 Kudos
3,957 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Rick

From below code, you can see that the emi_clk’s parent is pll2_pfd_400M, if we enable CONFIG_MX6_VPU_352M, then pll2_pfd_400M is actually running at 352M, so it can only be divided to 176M. Without CONFIG_MX6_VPU_352M, pll2_pfd_400M is running at 396M, so emi_clk can be at 198M.

5564 clk_set_parent(&emi_clk, &pll2_pfd_400M);

5565 #ifdef CONFIG_MX6_VPU_352M

5566 clk_set_rate(&emi_clk, 176000000);

5567 #else

5568 clk_set_rate(&emi_clk, 198000000);

5569 #endif

Best Regards.

Anson huang 黄勇才

Freescale Semiconductor Shanghai

上海浦东新区亮景路192号A座2楼

201203

Tel:021-28937058

0 Kudos
3,957 Views
rickchen
Contributor I

Hi Yongcai,

I am confused, since the config is increasing the frequency of VPU, But we decrease another clock. Does this means that emi_clk is not used so that we can use pll2_pfd_400M as input of vpu?

Thanks

0 Kudos
3,957 Views
AnsonHuang
NXP Employee
NXP Employee

The config is to increase VPU freq, after adding this config, VPU will source clock from pll2_pfd_400M. Please search the clock config code in clock.c with the VPU 352M config enabled. We did not intent to decrease the emi clock, but only because it's parent is set to 352M, can only be div to 176M, impossible to set to 198M.

Sent from my iPad

在 2013-11-4,20:04,"Rick Chen" <admin@community.freescale.com<mailto:admin@community.freescale.com>> 写道:

<https://community.freescale.com/>

<https://community.freescale.com/>

i.MX6Q: How to increase the VPU frequency?

reply from Rick Chen<https://community.freescale.com/people/rickchen?et=watches.email.thread> in i.MX Community - View the full discussion<https://community.freescale.com/message/360278?et=watches.email.thread#360278>

0 Kudos
3,957 Views
carlmichal
Contributor I

In LK 3.10, CONFIG_MX6_VPU_352M no longer affects any kernel code. It looks like the settings it used to affect are now accessible in userspace in /sys, but its not totally obvious (to me) which clock settings to change. I do see that bus scaling can be disabled in /sys/bus/platform/drivers/imx6_busfreq/busfreq.13/enable and the voltage can be increased in /sys/bus/platform/devices/soc.1/20000000.aips-bus/20c8000.anatop/...

But some advice on where the clk settings that need to be changed would be welcome.

0 Kudos
3,957 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Carl

     The latest patch for VPU 352M feature is as below, please check whether your code base has such commit:

commit 5af717749ea4df5bb77e15565758d5c12750356d
Author: Anson Huang <b20788@freescale.com>
Date:   Mon Jun 30 11:25:50 2014 +0800

    ENGR00320349 cpufreq: imx6: increase SOC/PU voltage for VPU352MHz
   
    For VPU352MHz enabled, SOC/PU voltage can NOT be lower than 1250mV,
    as only 396M and 792M setpoint's SOC/PU voltage is lower than
    1250mV and we already disable 396M setpoint, so here we just increase
    SOC/PU voltage for 792M setpoint when VPU352M is enabled.
   
    Signed-off-by: Anson Huang <b20788@freescale.com>

drivers/cpufreq/cpufreq-imx6.c

     The code change in clk code is as below, please check it whether it is in your code base, we do NOT support such feature until beta release.

arch/arm/mach-imx/clk-imx6q.c:

753 #ifdef CONFIG_MX6_VPU_352M

754         /*

755          * If VPU 352M is enabled, then PLL2_PDF2 need to be

756          * set to 352M, cpufreq will be disabled as VDDSOC/PU

757          * need to be at highest voltage, scaling cpu freq is

758          * not saving any power, and busfreq will be also disabled

759          * as the PLL2_PFD2 is not at default freq, in a word,

760          * all modules that sourceing clk from PLL2_PFD2 will

761          * be impacted.

762          */

763         imx_clk_set_rate(clk[pll2_pfd2_396m], 352000000);

764         imx_clk_set_parent(clk[vpu_axi_sel], clk[pll2_pfd2_396m]);

765         pr_info("VPU 352M is enabled!\n");

766 #endif

0 Kudos
3,957 Views
ralph__
Contributor IV

Hi, my arch/arm/mach-imx/clk-imx6q.c isn't even 766 lines long. I list my arch/arm/mach-imx/clk-imx6q.c file here - please could you tell me where I should insert the patch?

Thanks.

/*

* Copyright 2011-2014 Freescale Semiconductor, Inc.

* Copyright 2011 Linaro Ltd.

*

* The code contained herein is licensed under the GNU General Public

* License. You may obtain a copy of the GNU General Public License

* Version 2 or later at the following locations:

*

* http://www.opensource.org/licenses/gpl-license.html

* http://www.gnu.org/copyleft/gpl.html

*/

#include <linux/init.h>

#include <linux/types.h>

#include <linux/clk.h>

#include <linux/clkdev.h>

#include <linux/err.h>

#include <linux/io.h>

#include <linux/of.h>

#include <linux/of_address.h>

#include <linux/of_irq.h>

#include "clk.h"

#include "common.h"

#include "hardware.h"

#define CCM_CCGR_OFFSET(index)    (index * 2)

static const char *step_sels[]    = { "osc", "pll2_pfd2_396m", };

static const char *pll1_sw_sels[]    = { "pll1_sys", "step", };

static const char *periph_pre_sels[]    = { "pll2_bus", "pll2_pfd2_396m", "pll2_pfd0_352m", "pll2_198m", };

static const char *periph_clk2_sels[]    = { "pll3_usb_otg", "osc", "osc", "dummy", };

static const char *periph2_clk2_sels[]    = { "pll3_usb_otg", "pll2_bus", };

static const char *periph_sels[]    = { "periph_pre", "periph_clk2", };

static const char *periph2_sels[]    = { "periph2_pre", "periph2_clk2", };

static const char *axi_sels[]        = { "periph", "pll2_pfd2_396m", "periph", "pll3_pfd1_540m", };

static const char *audio_sels[]    = { "pll4_audio_div", "pll3_pfd2_508m", "pll3_pfd3_454m", "pll3_usb_otg", };

static const char *gpu_axi_sels[]    = { "axi", "ahb", };

static const char *gpu2d_core_sels[]    = { "axi", "pll3_usb_otg", "pll2_pfd0_352m", "pll2_pfd2_396m", };

static const char *gpu3d_core_sels[]    = { "mmdc_ch0_axi", "pll3_usb_otg", "pll2_pfd1_594m", "pll2_pfd2_396m", };

static const char *gpu3d_shader_sels[] = { "mmdc_ch0_axi", "pll3_usb_otg", "pll2_pfd1_594m", "pll3_pfd0_720m", };

static const char *ipu_sels[]        = { "mmdc_ch0_axi", "pll2_pfd2_396m", "pll3_120m", "pll3_pfd1_540m", };

static const char *ldb_di_sels[]    = { "pll5_video_div", "pll2_pfd0_352m", "pll2_pfd2_396m", "mmdc_ch1_axi", "pll3_usb_otg", };

static const char *ldb_di0_div_sels[]    = { "ldb_di0_div_3_5", "ldb_di0_div_7", };

static const char *ldb_di1_div_sels[]    = { "ldb_di1_div_3_5", "ldb_di1_div_7", };

static const char *ipu_di_pre_sels[]    = { "mmdc_ch0_axi", "pll3_usb_otg", "pll5_video_div", "pll2_pfd0_352m", "pll2_pfd2_396m", "pll3_pfd1_540m", };

static const char *ipu1_di0_sels[]    = { "ipu1_di0_pre", "dummy", "dummy", "ldb_di0", "ldb_di1", };

static const char *ipu1_di1_sels[]    = { "ipu1_di1_pre", "dummy", "dummy", "ldb_di0", "ldb_di1", };

static const char *ipu2_di0_sels[]    = { "ipu2_di0_pre", "dummy", "dummy", "ldb_di0", "ldb_di1", };

static const char *ipu2_di1_sels[]    = { "ipu2_di1_pre", "dummy", "dummy", "ldb_di0", "ldb_di1", };

static const char *hsi_tx_sels[]    = { "pll3_120m", "pll2_pfd2_396m", };

static const char *pcie_axi_sels[]    = { "axi", "ahb", };

static const char *ssi_sels[]        = { "pll3_pfd2_508m", "pll3_pfd3_454m", "pll4_audio_div", };

static const char *usdhc_sels[]    = { "pll2_pfd2_396m", "pll2_pfd0_352m", };

static const char *enfc_sels[]    = { "pll2_pfd0_352m", "pll2_bus", "pll3_usb_otg", "pll2_pfd2_396m", };

static const char *emi_sels[]        = { "pll2_pfd2_396m", "pll3_usb_otg", "axi", "pll2_pfd0_352m", };

static const char *emi_slow_sels[]      = { "axi", "pll3_usb_otg", "pll2_pfd2_396m", "pll2_pfd0_352m", };

static const char *vdo_axi_sels[]    = { "axi", "ahb", };

static const char *vpu_axi_sels[]    = { "axi", "pll2_pfd2_396m", "pll2_pfd0_352m", };

static const char *cko1_sels[]    = { "pll3_usb_otg", "pll2_bus", "pll1_sys", "pll5_video_div",

                    "dummy", "axi", "enfc", "ipu1_di0", "ipu1_di1", "ipu2_di0",

                    "ipu2_di1", "ahb", "ipg", "ipg_per", "ckil", "pll4_audio_div", };

static const char *cko2_sels[] = {

    "mmdc_ch0_axi", "mmdc_ch1_axi", "usdhc4", "usdhc1",

    "gpu2d_axi", "dummy", "ecspi_root", "gpu3d_axi",

    "usdhc3", "dummy", "arm", "ipu1",

    "ipu2", "vdo_axi", "osc", "gpu2d_core",

    "gpu3d_core", "usdhc2", "ssi1", "ssi2",

    "ssi3", "gpu3d_shader", "vpu_axi", "can_root",

    "ldb_di0", "ldb_di1", "esai", "eim_slow",

    "uart_serial", "spdif", "asrc", "hsi_tx",

};

static const char *cko_sels[] = { "cko1", "cko2", };

static const char *lvds_sels[]    = { "arm", "pll1_sys", "dummy", "dummy", "dummy", "dummy", "dummy", "pll5_video_div",

                    "dummy", "dummy", "pcie_ref", "sata_ref", "usbphy1", "usbphy2", };

static const char *pll_av_sels[] = { "osc", "lvds1_in", "lvds2_in", "dummy", };

static void __iomem *anatop_base;

static void __iomem *ccm_base;

enum mx6q_clks {

    dummy, ckil, ckih, osc, pll2_pfd0_352m, pll2_pfd1_594m, pll2_pfd2_396m,

    pll3_pfd0_720m, pll3_pfd1_540m, pll3_pfd2_508m, pll3_pfd3_454m,

    pll2_198m, pll3_120m, pll3_80m, pll3_60m, twd, step, pll1_sw,

    periph_pre, periph2_pre, periph_clk2_sel, periph2_clk2_sel, axi_sel,

    esai_sel, asrc_sel, spdif_sel, gpu2d_axi, gpu3d_axi, gpu2d_core_sel,

    gpu3d_core_sel, gpu3d_shader_sel, ipu1_sel, ipu2_sel, ldb_di0_sel,

    ldb_di1_sel, ipu1_di0_pre_sel, ipu1_di1_pre_sel, ipu2_di0_pre_sel,

    ipu2_di1_pre_sel, ipu1_di0_sel, ipu1_di1_sel, ipu2_di0_sel,

    ipu2_di1_sel, hsi_tx_sel, pcie_axi_sel, ssi1_sel, ssi2_sel, ssi3_sel,

    usdhc1_sel, usdhc2_sel, usdhc3_sel, usdhc4_sel, enfc_sel, emi_sel,

    emi_slow_sel, vdo_axi_sel, vpu_axi_sel, cko1_sel, periph, periph2,

    periph_clk2, periph2_clk2, ipg, ipg_per, esai_pred, esai_podf,

    asrc_pred, asrc_podf, spdif_pred, spdif_podf, can_root, ecspi_root,

    gpu2d_core_podf, gpu3d_core_podf, gpu3d_shader, ipu1_podf, ipu2_podf,

    ldb_di0_podf_unused, ldb_di1_podf_unused, ipu1_di0_pre, ipu1_di1_pre,

    ipu2_di0_pre, ipu2_di1_pre, hsi_tx_podf, ssi1_pred, ssi1_podf,

    ssi2_pred, ssi2_podf, ssi3_pred, ssi3_podf, uart_serial_podf,

    usdhc1_podf, usdhc2_podf, usdhc3_podf, usdhc4_podf, enfc_pred, enfc_podf,

    emi_podf, emi_slow_podf, vpu_axi_podf, cko1_podf, axi, mmdc_ch0_axi_podf,

    mmdc_ch1_axi_podf, arm, ahb, apbh_dma, asrc, can1_ipg, can1_serial,

    can2_ipg, can2_serial, ecspi1, ecspi2, ecspi3, ecspi4, ecspi5, enet,

    esai, gpt_ipg, gpt_ipg_per, gpu2d_core, gpu3d_core, hdmi_iahb,

    hdmi_isfr, i2c1, i2c2, i2c3, iim, enfc, ipu1, ipu1_di0, ipu1_di1, ipu2,

    ipu2_di0, ldb_di0, ldb_di1, ipu2_di1, hsi_tx, mlb, mmdc_ch0_axi,

    mmdc_ch1_axi, ocram, openvg_axi, pcie_axi, pwm1, pwm2, pwm3, pwm4, per1_bch,

    gpmi_bch_apb, gpmi_bch, gpmi_io, gpmi_apb, sata, sdma, spba, ssi1,

    ssi2, ssi3, uart_ipg, uart_serial, usboh3, usdhc1, usdhc2, usdhc3,

    usdhc4, vdo_axi, vpu_axi, cko1, pll1_sys, pll2_bus, pll3_usb_otg,

    pll4_audio, pll5_video, pll8_mlb, pll7_usb_host, pll6_enet, ssi1_ipg,

    ssi2_ipg, ssi3_ipg, rom, usbphy1, usbphy2, ldb_di0_div_3_5, ldb_di1_div_3_5,

    sata_ref, sata_ref_100m, pcie_ref, pcie_ref_125m, enet_ref, usbphy1_gate,

    usbphy2_gate, pll4_post_div, pll5_post_div, pll5_video_div, eim_slow,

    spdif, cko2_sel, cko2_podf, cko2, cko, vdoa, gpt_3m, video_27m,

    ldb_di0_div_7, ldb_di1_div_7, ldb_di0_div_sel, ldb_di1_div_sel,

    pll4_audio_div, lvds1_sel, lvds1_in, lvds1_out, caam_mem, caam_aclk,

    caam_ipg, epit1, epit2, tzasc2, pll4_sel, lvds2_sel, lvds2_in, lvds2_out,

    anaclk1, anaclk2, clk_max

};

static struct clk *clk[clk_max];

static struct clk_onecell_data clk_data;

static enum mx6q_clks const clks_init_on[] __initconst = {

    mmdc_ch0_axi, rom, arm,

};

static struct clk_div_table clk_enet_ref_table[] = {

    { .val = 0, .div = 20, },

    { .val = 1, .div = 10, },

    { .val = 2, .div = 5, },

    { .val = 3, .div = 4, },

};

static struct clk_div_table post_div_table[] = {

    { .val = 2, .div = 1, },

    { .val = 1, .div = 2, },

    { .val = 0, .div = 4, },

    { }

};

static struct clk_div_table video_div_table[] = {

    { .val = 0, .div = 1, },

    { .val = 1, .div = 2, },

    { .val = 2, .div = 1, },

    { .val = 3, .div = 4, },

    { }

};

static void init_ldb_clks(enum mx6q_clks new_parent)

{

    u32 reg;

    /*

     * Need to follow a strict procedure when changing the LDB

     * clock, else we can introduce a glitch. Things to keep in

     * mind:

     * 1. The current and new parent clocks must be disabled.

     * 2. The default clock for ldb_dio_clk is mmdc_ch1 which has

     * no CG bit.

     * 3. In the RTL implementation of the LDB_DI_CLK_SEL mux

     * the top four options are in one mux and the PLL3 option along

     * with another option is in the second mux. There is third mux

     * used to decide between the first and second mux.

     * The code below switches the parent to the bottom mux first

     * and then manipulates the top mux. This ensures that no glitch

     * will enter the divider.

     *

     * Need to disable MMDC_CH1 clock manually as there is no CG bit

     * for this clock. The only way to disable this clock is to move

     * it topll3_sw_clk and then to disable pll3_sw_clk

     * Make sure periph2_clk2_sel is set to pll3_sw_clk

     */

    reg = readl_relaxed(ccm_base + 0x18);

    reg &= ~(1 << 20);

    writel_relaxed(reg, ccm_base + 0x18);

    /*

     * Set MMDC_CH1 mask bit.

     */

    reg = readl_relaxed(ccm_base + 0x4);

    reg |= 1 << 16;

    writel_relaxed(reg, ccm_base + 0x4);

    /*

     * Set the periph2_clk_sel to the top mux so that

     * mmdc_ch1 is from pll3_sw_clk.

     */

    reg = readl_relaxed(ccm_base + 0x14);

    reg |= 1 << 26;

    writel_relaxed(reg, ccm_base + 0x14);

    /*

     * Wait for the clock switch.

     */

    while (readl_relaxed(ccm_base + 0x48))

        ;

    /*

     * Disable pll3_sw_clk by selecting the bypass clock source.

     */

    reg = readl_relaxed(ccm_base + 0xc);

    reg |= 1 << 0;

    writel_relaxed(reg, ccm_base + 0xc);

    /*

     * Set the ldb_di0_clk and ldb_di1_clk to 111b.

     */

    reg = readl_relaxed(ccm_base + 0x2c);

    reg |= ((7 << 9) | (7 << 12));

    writel_relaxed(reg, ccm_base + 0x2c);

    /*

     * Set the ldb_di0_clk and ldb_di1_clk to 100b.

     */

    reg = readl_relaxed(ccm_base + 0x2c);

    reg &= ~((7 << 9) | (7 << 12));

    reg |= ((4 << 9) | (4 << 12));

    writel_relaxed(reg, ccm_base + 0x2c);

    /*

     * Perform the LDB parent clock switch.

     */

    clk_set_parent(clk[ldb_di0_sel], clk[new_parent]);

    clk_set_parent(clk[ldb_di1_sel], clk[new_parent]);

    /*

     * Unbypass pll3_sw_clk.

     */

    reg = readl_relaxed(ccm_base + 0xc);

    reg &= ~(1 << 0);

    writel_relaxed(reg, ccm_base + 0xc);

    /*

     * Set the periph2_clk_sel back to the bottom mux so that

     * mmdc_ch1 is from its original parent.

     */

    reg = readl_relaxed(ccm_base + 0x14);

    reg &= ~(1 << 26);

    writel_relaxed(reg, ccm_base + 0x14);

    /*

     * Wait for the clock switch.

     */

    while (readl_relaxed(ccm_base + 0x48))

        ;

    /*

     * Clear MMDC_CH1 mask bit.

     */

    reg = readl_relaxed(ccm_base + 0x4);

    reg &= ~(1 << 16);

    writel_relaxed(reg, ccm_base + 0x4);

}

static void __init imx6q_clocks_init(struct device_node *ccm_node)

{

    struct device_node *np;

    void __iomem *base;

    int i, irq;

    int ret;

    u32 reg;

    clk[dummy] = imx_clk_fixed("dummy", 0);

    clk[ckil] = imx_obtain_fixed_clock("ckil", 0);

    clk[ckih] = imx_obtain_fixed_clock("ckih1", 0);

    clk[osc] = imx_obtain_fixed_clock("osc", 0);

    /* Clock source from external clock via ANACLK1/2 PADs */

    clk[anaclk1] = imx_obtain_fixed_clock("anaclk1", 0);

    clk[anaclk2] = imx_obtain_fixed_clock("anaclk2", 0);

    np = of_find_compatible_node(NULL, NULL, "fsl,imx6q-anatop");

    anatop_base = base = of_iomap(np, 0);

    WARN_ON(!base);

    /* Audio/video PLL post dividers do not work on i.MX6q revision 1.0 */

    if (cpu_is_imx6q() && imx_get_soc_revision() == IMX_CHIP_REVISION_1_0) {

        post_div_table[1].div = 1;

        post_div_table[2].div = 1;

        video_div_table[1].div = 1;

        video_div_table[2].div = 1;

    };

    /*                   type                               name         parent_name  base     div_mask */

    clk[pll1_sys]      = imx_clk_pllv3(IMX_PLLV3_SYS,    "pll1_sys",    "osc", base,        0x7f, false);

    clk[pll2_bus]      = imx_clk_pllv3(IMX_PLLV3_GENERIC,    "pll2_bus",    "osc", base + 0x30, 0x1, false);

    clk[pll3_usb_otg]  = imx_clk_pllv3(IMX_PLLV3_USB,    "pll3_usb_otg",    "osc", base + 0x10, 0x3, false);

    clk[pll4_audio]    = imx_clk_pllv3(IMX_PLLV3_AV,    "pll4_audio",    "pll4_sel", base + 0x70, 0x7f, false);

    clk[pll5_video]    = imx_clk_pllv3(IMX_PLLV3_AV,    "pll5_video",    "osc", base + 0xa0, 0x7f, false);

    clk[pll6_enet]     = imx_clk_pllv3(IMX_PLLV3_ENET,    "pll6_enet",    "osc", base + 0xe0, 0x3, false);

    clk[pll7_usb_host] = imx_clk_pllv3(IMX_PLLV3_USB,    "pll7_usb_host",    "osc", base + 0x20, 0x3, false);

    /*                              name            reg       shift width parent_names     num_parents */

    clk[lvds1_sel]    = imx_clk_mux("lvds1_sel",    base + 0x160, 0,  5,  lvds_sels,       ARRAY_SIZE(lvds_sels));

    clk[lvds2_sel]    = imx_clk_mux("lvds2_sel",    base + 0x160, 5,  5,  lvds_sels,       ARRAY_SIZE(lvds_sels));

    clk[pll4_sel]     = imx_clk_mux("pll4_sel",     base + 0x70, 14,  2,  pll_av_sels,     ARRAY_SIZE(pll_av_sels));

    /*

     * Bit 20 is the reserved and read-only bit, we do this only for:

     * - Do nothing for usbphy clk_enable/disable

     * - Keep refcount when do usbphy clk_enable/disable, in that case,

     * the clk framework may need to enable/disable usbphy's parent

     */

    clk[usbphy1] = imx_clk_gate("usbphy1", "pll3_usb_otg", base + 0x10, 20);

    clk[usbphy2] = imx_clk_gate("usbphy2", "pll7_usb_host", base + 0x20, 20);

    /*

     * usbphy*_gate needs to be on after system boots up, and software

     * never needs to control it anymore.

     */

    clk[usbphy1_gate] = imx_clk_gate("usbphy1_gate", "dummy", base + 0x10, 6);

    clk[usbphy2_gate] = imx_clk_gate("usbphy2_gate", "dummy", base + 0x20, 6);

    clk[sata_ref] = imx_clk_fixed_factor("sata_ref", "pll6_enet", 1, 5);

    clk[pcie_ref] = imx_clk_fixed_factor("pcie_ref", "pll6_enet", 1, 4);

    /* NOTICE: The gate of the lvds1/2 in/out is used to select the clk direction */

    clk[lvds1_in] = imx_clk_gate("lvds1_in", "anaclk1", base + 0x160, 12);

    clk[lvds2_in] = imx_clk_gate("lvds2_in", "anaclk2", base + 0x160, 13);

    clk[lvds1_out] = imx_clk_gate("lvds1_out", "lvds1_sel", base + 0x160, 10);

    clk[lvds2_out] = imx_clk_gate("lvds2_out", "lvds2_sel", base + 0x160, 11);

    clk[sata_ref_100m] = imx_clk_gate("sata_ref_100m", "sata_ref", base + 0xe0, 20);

    clk[pcie_ref_125m] = imx_clk_gate("pcie_ref_125m", "pcie_ref", base + 0xe0, 19);

    clk[enet_ref] = clk_register_divider_table(NULL, "enet_ref", "pll6_enet", 0,

            base + 0xe0, 0, 2, 0, clk_enet_ref_table,

            &imx_ccm_lock);

    /*                                name              parent_name        reg       idx */

    clk[pll2_pfd0_352m] = imx_clk_pfd("pll2_pfd0_352m", "pll2_bus",     base + 0x100, 0);

    clk[pll2_pfd1_594m] = imx_clk_pfd("pll2_pfd1_594m", "pll2_bus",     base + 0x100, 1);

    clk[pll2_pfd2_396m] = imx_clk_pfd("pll2_pfd2_396m", "pll2_bus",     base + 0x100, 2);

    clk[pll3_pfd0_720m] = imx_clk_pfd("pll3_pfd0_720m", "pll3_usb_otg", base + 0xf0,  0);

    clk[pll3_pfd1_540m] = imx_clk_pfd("pll3_pfd1_540m", "pll3_usb_otg", base + 0xf0,  1);

    clk[pll3_pfd2_508m] = imx_clk_pfd("pll3_pfd2_508m", "pll3_usb_otg", base + 0xf0,  2);

    clk[pll3_pfd3_454m] = imx_clk_pfd("pll3_pfd3_454m", "pll3_usb_otg", base + 0xf0,  3);

    /*                                    name         parent_name     mult div */

    clk[pll2_198m] = imx_clk_fixed_factor("pll2_198m", "pll2_pfd2_396m", 1, 2);

    clk[pll3_120m] = imx_clk_fixed_factor("pll3_120m", "pll3_usb_otg",   1, 4);

    clk[pll3_80m]  = imx_clk_fixed_factor("pll3_80m",  "pll3_usb_otg",   1, 6);

    clk[pll3_60m]  = imx_clk_fixed_factor("pll3_60m",  "pll3_usb_otg",   1, 8);

    clk[twd]       = imx_clk_fixed_factor("twd",       "arm",            1, 2);

    clk[gpt_3m]    = imx_clk_fixed_factor("gpt_3m",    "osc",            1, 8);

    clk[video_27m] = imx_clk_fixed_factor("video_27m", "pll3_pfd1_540m", 1, 20);

    clk[pll4_post_div] = clk_register_divider_table(NULL, "pll4_post_div", "pll4_audio", CLK_SET_RATE_PARENT, base + 0x70, 19, 2, 0, post_div_table, &imx_ccm_lock);

    clk[pll4_audio_div] = clk_register_divider(NULL, "pll4_audio_div", "pll4_post_div", CLK_SET_RATE_PARENT, base + 0x170, 15, 1, 0, &imx_ccm_lock);

    clk[pll5_post_div] = clk_register_divider_table(NULL, "pll5_post_div", "pll5_video", CLK_SET_RATE_PARENT, base + 0xa0, 19, 2, 0, post_div_table, &imx_ccm_lock);

    clk[pll5_video_div] = clk_register_divider_table(NULL, "pll5_video_div", "pll5_post_div", CLK_SET_RATE_PARENT, base + 0x170, 30, 2, 0, video_div_table, &imx_ccm_lock);

    np = ccm_node;

    ccm_base = base = of_iomap(np, 0);

    WARN_ON(!base);

    imx6_pm_set_ccm_base(base);

    /*                                  name                reg       shift width parent_names     num_parents */

    clk[step]             = imx_clk_mux("step",            base + 0xc,  8,  1, step_sels,           ARRAY_SIZE(step_sels));

    clk[pll1_sw]          = imx_clk_mux("pll1_sw",            base + 0xc,  2,  1, pll1_sw_sels,      ARRAY_SIZE(pll1_sw_sels));

    clk[periph_pre]       = imx_clk_mux("periph_pre",       base + 0x18, 18, 2, periph_pre_sels,   ARRAY_SIZE(periph_pre_sels));

    clk[periph2_pre]      = imx_clk_mux("periph2_pre",      base + 0x18, 21, 2, periph_pre_sels,   ARRAY_SIZE(periph_pre_sels));

    clk[periph_clk2_sel]  = imx_clk_mux("periph_clk2_sel",  base + 0x18, 12, 2, periph_clk2_sels,  ARRAY_SIZE(periph_clk2_sels));

    clk[periph2_clk2_sel] = imx_clk_mux("periph2_clk2_sel", base + 0x18, 20, 1, periph2_clk2_sels, ARRAY_SIZE(periph2_clk2_sels));

    clk[axi_sel]          = imx_clk_mux("axi_sel",          base + 0x14, 6,  2, axi_sels,          ARRAY_SIZE(axi_sels));

    clk[esai_sel]         = imx_clk_mux("esai_sel",         base + 0x20, 19, 2, audio_sels,        ARRAY_SIZE(audio_sels));

    clk[asrc_sel]         = imx_clk_mux("asrc_sel",         base + 0x30, 7,  2, audio_sels,        ARRAY_SIZE(audio_sels));

    clk[spdif_sel]        = imx_clk_mux("spdif_sel",        base + 0x30, 20, 2, audio_sels,        ARRAY_SIZE(audio_sels));

    clk[gpu2d_axi]        = imx_clk_mux("gpu2d_axi",        base + 0x18, 0,  1, gpu_axi_sels,      ARRAY_SIZE(gpu_axi_sels));

    clk[gpu3d_axi]        = imx_clk_mux("gpu3d_axi",        base + 0x18, 1,  1, gpu_axi_sels,      ARRAY_SIZE(gpu_axi_sels));

    clk[gpu2d_core_sel]   = imx_clk_mux("gpu2d_core_sel",   base + 0x18, 16, 2, gpu2d_core_sels,   ARRAY_SIZE(gpu2d_core_sels));

    clk[gpu3d_core_sel]   = imx_clk_mux("gpu3d_core_sel",   base + 0x18, 4,  2, gpu3d_core_sels,   ARRAY_SIZE(gpu3d_core_sels));

    clk[gpu3d_shader_sel] = imx_clk_mux("gpu3d_shader_sel", base + 0x18, 8,  2, gpu3d_shader_sels, ARRAY_SIZE(gpu3d_shader_sels));

    clk[ipu1_sel]         = imx_clk_mux("ipu1_sel",         base + 0x3c, 9,  2, ipu_sels,          ARRAY_SIZE(ipu_sels));

    clk[ipu2_sel]         = imx_clk_mux("ipu2_sel",         base + 0x3c, 14, 2, ipu_sels,          ARRAY_SIZE(ipu_sels));

    clk[ldb_di0_sel]      = imx_clk_mux_flags("ldb_di0_sel", base + 0x2c, 9,  3, ldb_di_sels,      ARRAY_SIZE(ldb_di_sels), CLK_SET_RATE_PARENT);

    clk[ldb_di1_sel]      = imx_clk_mux_flags("ldb_di1_sel", base + 0x2c, 12, 3, ldb_di_sels,      ARRAY_SIZE(ldb_di_sels), CLK_SET_RATE_PARENT);

    clk[ldb_di0_div_sel]  = imx_clk_mux_flags("ldb_di0_div_sel", base + 0x20, 10, 1, ldb_di0_div_sels, ARRAY_SIZE(ldb_di0_div_sels), CLK_SET_RATE_PARENT);

    clk[ldb_di1_div_sel]  = imx_clk_mux_flags("ldb_di1_div_sel", base + 0x20, 11, 1, ldb_di1_div_sels, ARRAY_SIZE(ldb_di1_div_sels), CLK_SET_RATE_PARENT);

    clk[ipu1_di0_pre_sel] = imx_clk_mux_flags("ipu1_di0_pre_sel", base + 0x34, 6,  3, ipu_di_pre_sels,   ARRAY_SIZE(ipu_di_pre_sels), CLK_SET_RATE_PARENT);

    clk[ipu1_di1_pre_sel] = imx_clk_mux_flags("ipu1_di1_pre_sel", base + 0x34, 15, 3, ipu_di_pre_sels,   ARRAY_SIZE(ipu_di_pre_sels), CLK_SET_RATE_PARENT);

    clk[ipu2_di0_pre_sel] = imx_clk_mux_flags("ipu2_di0_pre_sel", base + 0x38, 6,  3, ipu_di_pre_sels,   ARRAY_SIZE(ipu_di_pre_sels), CLK_SET_RATE_PARENT);

    clk[ipu2_di1_pre_sel] = imx_clk_mux_flags("ipu2_di1_pre_sel", base + 0x38, 15, 3, ipu_di_pre_sels,   ARRAY_SIZE(ipu_di_pre_sels), CLK_SET_RATE_PARENT);

    clk[ipu1_di0_sel]     = imx_clk_mux_flags("ipu1_di0_sel",     base + 0x34, 0,  3, ipu1_di0_sels,     ARRAY_SIZE(ipu1_di0_sels), CLK_SET_RATE_PARENT);

    clk[ipu1_di1_sel]     = imx_clk_mux_flags("ipu1_di1_sel",     base + 0x34, 9,  3, ipu1_di1_sels,     ARRAY_SIZE(ipu1_di1_sels), CLK_SET_RATE_PARENT);

    clk[ipu2_di0_sel]     = imx_clk_mux_flags("ipu2_di0_sel",     base + 0x38, 0,  3, ipu2_di0_sels,     ARRAY_SIZE(ipu2_di0_sels), CLK_SET_RATE_PARENT);

    clk[ipu2_di1_sel]     = imx_clk_mux_flags("ipu2_di1_sel",     base + 0x38, 9,  3, ipu2_di1_sels,     ARRAY_SIZE(ipu2_di1_sels), CLK_SET_RATE_PARENT);

    clk[hsi_tx_sel]       = imx_clk_mux("hsi_tx_sel",       base + 0x30, 28, 1, hsi_tx_sels,       ARRAY_SIZE(hsi_tx_sels));

    clk[pcie_axi_sel]     = imx_clk_mux("pcie_axi_sel",     base + 0x18, 10, 1, pcie_axi_sels,     ARRAY_SIZE(pcie_axi_sels));

    clk[ssi1_sel]         = imx_clk_fixup_mux("ssi1_sel",   base + 0x1c, 10, 2, ssi_sels,          ARRAY_SIZE(ssi_sels),          imx_cscmr1_fixup);

    clk[ssi2_sel]         = imx_clk_fixup_mux("ssi2_sel",   base + 0x1c, 12, 2, ssi_sels,          ARRAY_SIZE(ssi_sels),          imx_cscmr1_fixup);

    clk[ssi3_sel]         = imx_clk_fixup_mux("ssi3_sel",   base + 0x1c, 14, 2, ssi_sels,          ARRAY_SIZE(ssi_sels),          imx_cscmr1_fixup);

    clk[usdhc1_sel]       = imx_clk_fixup_mux("usdhc1_sel", base + 0x1c, 16, 1, usdhc_sels,        ARRAY_SIZE(usdhc_sels),        imx_cscmr1_fixup);

    clk[usdhc2_sel]       = imx_clk_fixup_mux("usdhc2_sel", base + 0x1c, 17, 1, usdhc_sels,        ARRAY_SIZE(usdhc_sels),        imx_cscmr1_fixup);

    clk[usdhc3_sel]       = imx_clk_fixup_mux("usdhc3_sel", base + 0x1c, 18, 1, usdhc_sels,        ARRAY_SIZE(usdhc_sels),        imx_cscmr1_fixup);

    clk[usdhc4_sel]       = imx_clk_fixup_mux("usdhc4_sel", base + 0x1c, 19, 1, usdhc_sels,        ARRAY_SIZE(usdhc_sels),        imx_cscmr1_fixup);

    clk[enfc_sel]         = imx_clk_mux("enfc_sel",         base + 0x2c, 16, 2, enfc_sels,         ARRAY_SIZE(enfc_sels));

    clk[emi_sel]          = imx_clk_fixup_mux("emi_sel",      base + 0x1c, 27, 2, emi_sels,        ARRAY_SIZE(emi_sels),          imx_cscmr1_fixup);

    clk[emi_slow_sel]     = imx_clk_fixup_mux("emi_slow_sel", base + 0x1c, 29, 2, emi_slow_sels,   ARRAY_SIZE(emi_slow_sels),     imx_cscmr1_fixup);

    clk[vdo_axi_sel]      = imx_clk_mux("vdo_axi_sel",      base + 0x18, 11, 1, vdo_axi_sels,      ARRAY_SIZE(vdo_axi_sels));

    clk[vpu_axi_sel]      = imx_clk_mux("vpu_axi_sel",      base + 0x18, 14, 2, vpu_axi_sels,      ARRAY_SIZE(vpu_axi_sels));

    clk[cko1_sel]         = imx_clk_mux("cko1_sel",         base + 0x60, 0,  4, cko1_sels,         ARRAY_SIZE(cko1_sels));

    clk[cko2_sel]         = imx_clk_mux("cko2_sel",         base + 0x60, 16, 5, cko2_sels,         ARRAY_SIZE(cko2_sels));

    clk[cko]              = imx_clk_mux("cko",              base + 0x60, 8, 1,  cko_sels,          ARRAY_SIZE(cko_sels));

    /*                              name         reg      shift width busy: reg, shift parent_names  num_parents */

    clk[periph]  = imx_clk_busy_mux("periph",  base + 0x14, 25,  1,   base + 0x48, 5,  periph_sels,  ARRAY_SIZE(periph_sels));

    clk[periph2] = imx_clk_busy_mux("periph2", base + 0x14, 26,  1,   base + 0x48, 3,  periph2_sels, ARRAY_SIZE(periph2_sels));

    /*                                      name                parent_name          reg       shift width */

    clk[periph_clk2]      = imx_clk_divider("periph_clk2",      "periph_clk2_sel",   base + 0x14, 27, 3);

    clk[periph2_clk2]     = imx_clk_divider("periph2_clk2",     "periph2_clk2_sel",  base + 0x14, 0,  3);

    clk[ipg]              = imx_clk_divider("ipg",              "ahb",               base + 0x14, 8,  2);

    clk[ipg_per]          = imx_clk_fixup_divider("ipg_per",    "ipg",               base + 0x1c, 0,  6, imx_cscmr1_fixup);

    clk[esai_pred]        = imx_clk_divider("esai_pred",        "esai_sel",          base + 0x28, 9,  3);

    clk[esai_podf]        = imx_clk_divider("esai_podf",        "esai_pred",         base + 0x28, 25, 3);

    clk[asrc_pred]        = imx_clk_divider("asrc_pred",        "asrc_sel",          base + 0x30, 12, 3);

    clk[asrc_podf]        = imx_clk_divider("asrc_podf",        "asrc_pred",         base + 0x30, 9,  3);

    clk[spdif_pred]       = imx_clk_divider("spdif_pred",       "spdif_sel",         base + 0x30, 25, 3);

    clk[spdif_podf]       = imx_clk_divider("spdif_podf",       "spdif_pred",        base + 0x30, 22, 3);

    clk[can_root]         = imx_clk_divider("can_root",         "pll3_60m",          base + 0x20, 2,  6);

    clk[ecspi_root]       = imx_clk_divider("ecspi_root",       "pll3_60m",          base + 0x38, 19, 6);

    clk[gpu2d_core_podf]  = imx_clk_divider("gpu2d_core_podf",  "gpu2d_core_sel",    base + 0x18, 23, 3);

    clk[gpu3d_core_podf]  = imx_clk_divider("gpu3d_core_podf",  "gpu3d_core_sel",    base + 0x18, 26, 3);

    clk[gpu3d_shader]     = imx_clk_divider("gpu3d_shader",     "gpu3d_shader_sel",  base + 0x18, 29, 3);

    clk[ipu1_podf]        = imx_clk_divider("ipu1_podf",        "ipu1_sel",          base + 0x3c, 11, 3);

    clk[ipu2_podf]        = imx_clk_divider("ipu2_podf",        "ipu2_sel",          base + 0x3c, 16, 3);

    clk[ldb_di0_div_3_5]  = imx_clk_fixed_factor("ldb_di0_div_3_5", "ldb_di0_sel", 2, 7);

    clk[ldb_di0_div_7]    = imx_clk_fixed_factor("ldb_di0_div_7",   "ldb_di0_sel", 1, 7);

    clk[ldb_di1_div_3_5]  = imx_clk_fixed_factor("ldb_di1_div_3_5", "ldb_di1_sel", 2, 7);

    clk[ldb_di1_div_7]    = imx_clk_fixed_factor("ldb_di1_div_7",   "ldb_di1_sel", 1, 7);

    clk[ipu1_di0_pre]     = imx_clk_divider("ipu1_di0_pre",     "ipu1_di0_pre_sel",  base + 0x34, 3,  3);

    clk[ipu1_di1_pre]     = imx_clk_divider("ipu1_di1_pre",     "ipu1_di1_pre_sel",  base + 0x34, 12, 3);

    clk[ipu2_di0_pre]     = imx_clk_divider("ipu2_di0_pre",     "ipu2_di0_pre_sel",  base + 0x38, 3,  3);

    clk[ipu2_di1_pre]     = imx_clk_divider("ipu2_di1_pre",     "ipu2_di1_pre_sel",  base + 0x38, 12, 3);

    clk[hsi_tx_podf]      = imx_clk_divider("hsi_tx_podf",      "hsi_tx_sel",        base + 0x30, 29, 3);

    clk[ssi1_pred]        = imx_clk_divider("ssi1_pred",        "ssi1_sel",          base + 0x28, 6,  3);

    clk[ssi1_podf]        = imx_clk_divider("ssi1_podf",        "ssi1_pred",         base + 0x28, 0,  6);

    clk[ssi2_pred]        = imx_clk_divider("ssi2_pred",        "ssi2_sel",          base + 0x2c, 6,  3);

    clk[ssi2_podf]        = imx_clk_divider("ssi2_podf",        "ssi2_pred",         base + 0x2c, 0,  6);

    clk[ssi3_pred]        = imx_clk_divider("ssi3_pred",        "ssi3_sel",          base + 0x28, 22, 3);

    clk[ssi3_podf]        = imx_clk_divider("ssi3_podf",        "ssi3_pred",         base + 0x28, 16, 6);

    clk[uart_serial_podf] = imx_clk_divider("uart_serial_podf", "pll3_80m",          base + 0x24, 0,  6);

    clk[usdhc1_podf]      = imx_clk_divider("usdhc1_podf",      "usdhc1_sel",        base + 0x24, 11, 3);

    clk[usdhc2_podf]      = imx_clk_divider("usdhc2_podf",      "usdhc2_sel",        base + 0x24, 16, 3);

    clk[usdhc3_podf]      = imx_clk_divider("usdhc3_podf",      "usdhc3_sel",        base + 0x24, 19, 3);

    clk[usdhc4_podf]      = imx_clk_divider("usdhc4_podf",      "usdhc4_sel",        base + 0x24, 22, 3);

    clk[enfc_pred]        = imx_clk_divider("enfc_pred",        "enfc_sel",          base + 0x2c, 18, 3);

    clk[enfc_podf]        = imx_clk_divider("enfc_podf",        "enfc_pred",         base + 0x2c, 21, 6);

    clk[emi_podf]         = imx_clk_fixup_divider("emi_podf",   "emi_sel",           base + 0x1c, 20, 3, imx_cscmr1_fixup);

    clk[emi_slow_podf]    = imx_clk_fixup_divider("emi_slow_podf", "emi_slow_sel",   base + 0x1c, 23, 3, imx_cscmr1_fixup);

    clk[vpu_axi_podf]     = imx_clk_divider("vpu_axi_podf",     "vpu_axi_sel",       base + 0x24, 25, 3);

    clk[cko1_podf]        = imx_clk_divider("cko1_podf",        "cko1_sel",          base + 0x60, 4,  3);

    clk[cko2_podf]        = imx_clk_divider("cko2_podf",        "cko2_sel",          base + 0x60, 21, 3);

    /*                                            name                 parent_name    reg        shift width busy: reg, shift */

    clk[axi]               = imx_clk_busy_divider("axi",               "axi_sel",     base + 0x14, 16,  3,   base + 0x48, 0);

    clk[mmdc_ch0_axi_podf] = imx_clk_busy_divider("mmdc_ch0_axi_podf", "periph",      base + 0x14, 19,  3,   base + 0x48, 4);

    clk[mmdc_ch1_axi_podf] = imx_clk_busy_divider("mmdc_ch1_axi_podf", "periph2",     base + 0x14, 3,   3,   base + 0x48, 2);

    clk[arm]               = imx_clk_busy_divider("arm",               "pll1_sw",     base + 0x10, 0,   3,   base + 0x48, 16);

    clk[ahb]               = imx_clk_busy_divider("ahb",               "periph",      base + 0x14, 10,  3,   base + 0x48, 1);

    /*                                name             parent_name          reg         shift */

    clk[apbh_dma]     = imx_clk_gate2("apbh_dma",      "usdhc3",            base + 0x68, 4);

    clk[asrc]         = imx_clk_gate2("asrc",          "asrc_podf",         base + 0x68, 6);

    clk[caam_mem]     = imx_clk_gate2("caam_mem",      "ahb",               base + 0x68, 8);

    clk[caam_aclk]    = imx_clk_gate2("caam_aclk",     "ahb",               base + 0x68, 10);

    clk[caam_ipg]     = imx_clk_gate2("caam_ipg",      "ipg",               base + 0x68, 12);

    clk[can1_ipg]     = imx_clk_gate2("can1_ipg",      "ipg",               base + 0x68, 14);

    clk[can1_serial]  = imx_clk_gate2("can1_serial",   "can_root",          base + 0x68, 16);

    clk[can2_ipg]     = imx_clk_gate2("can2_ipg",      "ipg",               base + 0x68, 18);

    clk[can2_serial]  = imx_clk_gate2("can2_serial",   "can_root",          base + 0x68, 20);

    clk[ecspi1]       = imx_clk_gate2("ecspi1",        "ecspi_root",        base + 0x6c, 0);

    clk[ecspi2]       = imx_clk_gate2("ecspi2",        "ecspi_root",        base + 0x6c, 2);

    clk[ecspi3]       = imx_clk_gate2("ecspi3",        "ecspi_root",        base + 0x6c, 4);

    clk[ecspi4]       = imx_clk_gate2("ecspi4",        "ecspi_root",        base + 0x6c, 6);

    clk[ecspi5]       = imx_clk_gate2("ecspi5",        "ecspi_root",        base + 0x6c, 8);

    clk[enet]         = imx_clk_gate2("enet",          "ipg",               base + 0x6c, 10);

    clk[epit1]        = imx_clk_gate2("epit1",         "ipg",               base + 0x6c, 12);

    clk[epit2]        = imx_clk_gate2("epit2",         "ipg",               base + 0x6c, 14);

    clk[esai]         = imx_clk_gate2("esai",          "esai_podf",         base + 0x6c, 16);

    clk[gpt_ipg]      = imx_clk_gate2("gpt_ipg",       "ipg",               base + 0x6c, 20);

    clk[gpt_ipg_per]  = imx_clk_gate2("gpt_ipg_per",   "ipg_per",           base + 0x6c, 22);

    if (cpu_is_imx6dl())

        /*

         * The multiplexer and divider of imx6q clock gpu3d_shader get

         * redefined/reused as gpu2d_core_sel and gpu2d_core_podf on imx6dl.

         */

        clk[gpu2d_core] = imx_clk_gate2("gpu2d_core", "gpu3d_shader", base + 0x6c, 24);

    else

        clk[gpu2d_core] = imx_clk_gate2("gpu2d_core", "gpu2d_core_podf", base + 0x6c, 24);

    clk[gpu3d_core]   = imx_clk_gate2("gpu3d_core",    "gpu3d_core_podf",   base + 0x6c, 26);

    clk[hdmi_iahb]    = imx_clk_gate2("hdmi_iahb",     "ahb",               base + 0x70, 0);

    clk[hdmi_isfr]    = imx_clk_gate2("hdmi_isfr",     "pll3_pfd1_540m",    base + 0x70, 4);

    clk[i2c1]         = imx_clk_gate2("i2c1",          "ipg_per",           base + 0x70, 6);

    clk[i2c2]         = imx_clk_gate2("i2c2",          "ipg_per",           base + 0x70, 8);

    clk[i2c3]         = imx_clk_gate2("i2c3",          "ipg_per",           base + 0x70, 10);

    clk[iim]          = imx_clk_gate2("iim",           "ipg",               base + 0x70, 12);

    clk[enfc]         = imx_clk_gate2("enfc",          "enfc_podf",         base + 0x70, 14);

    clk[tzasc2]       = imx_clk_gate2("tzasc2",        "mmdc_ch0_axi_podf", base + 0x70, 24);

    clk[vdoa]         = imx_clk_gate2("vdoa",          "vdo_axi",           base + 0x70, 26);

    clk[ipu1]         = imx_clk_gate2("ipu1",          "ipu1_podf",         base + 0x74, 0);

    clk[ipu1_di0]     = imx_clk_gate2("ipu1_di0",      "ipu1_di0_sel",      base + 0x74, 2);

    clk[ipu1_di1]     = imx_clk_gate2("ipu1_di1",      "ipu1_di1_sel",      base + 0x74, 4);

    clk[ipu2]         = imx_clk_gate2("ipu2",          "ipu2_podf",         base + 0x74, 6);

    clk[ipu2_di0]     = imx_clk_gate2("ipu2_di0",      "ipu2_di0_sel",      base + 0x74, 8);

    clk[ipu2_di1]     = imx_clk_gate2("ipu2_di1",      "ipu2_di1_sel",      base + 0x74, 10);

    clk[ldb_di0]      = imx_clk_gate2("ldb_di0",       "ldb_di0_div_sel",   base + 0x74, 12);

    clk[ldb_di1]      = imx_clk_gate2("ldb_di1",       "ldb_di1_div_sel",   base + 0x74, 14);

    clk[hsi_tx]       = imx_clk_gate2("hsi_tx",        "hsi_tx_podf",       base + 0x74, 16);

    if (cpu_is_imx6dl())

        /*

         * The multiplexer and divider of the imx6q clock gpu2d get

         * redefined/reused as mlb_sys_sel and mlb_sys_clk_podf on imx6dl.

         */

        clk[mlb] = imx_clk_gate2("mlb",            "gpu2d_core_podf",   base + 0x74, 18);

    else

        clk[mlb] = imx_clk_gate2("mlb",            "axi",               base + 0x74, 18);

    clk[mmdc_ch0_axi] = imx_clk_gate2("mmdc_ch0_axi",  "mmdc_ch0_axi_podf", base + 0x74, 20);

    clk[mmdc_ch1_axi] = imx_clk_gate2("mmdc_ch1_axi",  "mmdc_ch1_axi_podf", base + 0x74, 22);

    clk[ocram]        = imx_clk_gate2("ocram",         "ahb",               base + 0x74, 28);

    clk[openvg_axi]   = imx_clk_gate2("openvg_axi",    "axi",               base + 0x74, 30);

    clk[pcie_axi]     = imx_clk_gate2("pcie_axi",      "pcie_axi_sel",      base + 0x78, 0);

    clk[per1_bch]     = imx_clk_gate2("per1_bch",      "usdhc3",            base + 0x78, 12);

    clk[pwm1]         = imx_clk_gate2("pwm1",          "ipg_per",           base + 0x78, 16);

    clk[pwm2]         = imx_clk_gate2("pwm2",          "ipg_per",           base + 0x78, 18);

    clk[pwm3]         = imx_clk_gate2("pwm3",          "ipg_per",           base + 0x78, 20);

    clk[pwm4]         = imx_clk_gate2("pwm4",          "ipg_per",           base + 0x78, 22);

    clk[gpmi_bch_apb] = imx_clk_gate2("gpmi_bch_apb",  "usdhc3",            base + 0x78, 24);

    clk[gpmi_bch]     = imx_clk_gate2("gpmi_bch",      "usdhc4",            base + 0x78, 26);

    clk[gpmi_io]      = imx_clk_gate2("gpmi_io",       "enfc",              base + 0x78, 28);

    clk[gpmi_apb]     = imx_clk_gate2("gpmi_apb",      "usdhc3",            base + 0x78, 30);

    clk[rom]          = imx_clk_gate2("rom",           "ahb",               base + 0x7c, 0);

    clk[sata]         = imx_clk_gate2("sata",          "ipg",               base + 0x7c, 4);

    clk[sdma]         = imx_clk_gate2("sdma",          "ahb",               base + 0x7c, 6);

    clk[spba]         = imx_clk_gate2("spba",          "ipg",               base + 0x7c, 12);

    clk[spdif]        = imx_clk_gate2("spdif",         "spdif_podf",        base + 0x7c, 14);

    clk[ssi1_ipg]     = imx_clk_gate2("ssi1_ipg",      "ipg",               base + 0x7c, 18);

    clk[ssi2_ipg]     = imx_clk_gate2("ssi2_ipg",      "ipg",               base + 0x7c, 20);

    clk[ssi3_ipg]     = imx_clk_gate2("ssi3_ipg",      "ipg",               base + 0x7c, 22);

    clk[ssi1]         = imx_clk_gate2("ssi1",          "ssi1_podf",         base + 0x7c, 18);

    clk[ssi2]         = imx_clk_gate2("ssi2",          "ssi2_podf",         base + 0x7c, 20);

    clk[ssi3]         = imx_clk_gate2("ssi3",          "ssi3_podf",         base + 0x7c, 22);

    clk[uart_ipg]     = imx_clk_gate2("uart_ipg",      "ipg",               base + 0x7c, 24);

    clk[uart_serial]  = imx_clk_gate2("uart_serial",   "uart_serial_podf",  base + 0x7c, 26);

    clk[usboh3]       = imx_clk_gate2("usboh3",        "ipg",               base + 0x80, 0);

    clk[usdhc1]       = imx_clk_gate2("usdhc1",        "usdhc1_podf",       base + 0x80, 2);

    clk[usdhc2]       = imx_clk_gate2("usdhc2",        "usdhc2_podf",       base + 0x80, 4);

    clk[usdhc3]       = imx_clk_gate2("usdhc3",        "usdhc3_podf",       base + 0x80, 6);

    clk[usdhc4]       = imx_clk_gate2("usdhc4",        "usdhc4_podf",       base + 0x80, 8);

    clk[eim_slow]     = imx_clk_gate2("eim_slow",      "emi_slow_podf",     base + 0x80, 10);

    clk[vdo_axi]      = imx_clk_gate2("vdo_axi",       "vdo_axi_sel",       base + 0x80, 12);

    clk[vpu_axi]      = imx_clk_gate2("vpu_axi",       "vpu_axi_podf",      base + 0x80, 14);

    clk[cko1]         = imx_clk_gate("cko1",           "cko1_podf",         base + 0x60, 7);

    clk[cko2]         = imx_clk_gate("cko2",           "cko2_podf",         base + 0x60, 24);

    for (i = 0; i < ARRAY_SIZE(clk); i++)

        if (IS_ERR(clk[i]))

            pr_err("i.MX6q clk %d: register failed with %ld\n",

                i, PTR_ERR(clk[i]));

    /* Initialize clock gate status */

    writel_relaxed(1 << CCM_CCGR_OFFSET(11) |

        3 << CCM_CCGR_OFFSET(1) |

        3 << CCM_CCGR_OFFSET(0), base + 0x68);

    if (cpu_is_imx6q() && imx_get_soc_revision() == IMX_CHIP_REVISION_1_0)

        writel_relaxed(3 << CCM_CCGR_OFFSET(11) |

            3 << CCM_CCGR_OFFSET(10), base + 0x6c);

    else

        writel_relaxed(3 << CCM_CCGR_OFFSET(10), base + 0x6c);

    writel_relaxed(1 << CCM_CCGR_OFFSET(12) |

        3 << CCM_CCGR_OFFSET(11) |

        3 << CCM_CCGR_OFFSET(10) |

        3 << CCM_CCGR_OFFSET(9) |

        3 << CCM_CCGR_OFFSET(8), base + 0x70);

    writel_relaxed(3 << CCM_CCGR_OFFSET(14) |

        1 << CCM_CCGR_OFFSET(13) |

        3 << CCM_CCGR_OFFSET(12) |

        1 << CCM_CCGR_OFFSET(11) |

        3 << CCM_CCGR_OFFSET(10), base + 0x74);

    writel_relaxed(3 << CCM_CCGR_OFFSET(7) |

        3 << CCM_CCGR_OFFSET(6) |

        3 << CCM_CCGR_OFFSET(4), base + 0x78);

    writel_relaxed(1 << CCM_CCGR_OFFSET(0), base + 0x7c);

    writel_relaxed(0, base + 0x80);

    /* Make sure PFDs are disabled at boot. */

    reg = readl_relaxed(anatop_base + 0x100);

    /* Cannot disable pll2_pfd2_396M, as it is the MMDC clock in iMX6DL */

    if (cpu_is_imx6dl())

        reg |= 0x80008080;

    else

        reg |= 0x80808080;

    writel_relaxed(reg, anatop_base + 0x100);

    /* Disable PLL3 PFDs. */

    reg = readl_relaxed(anatop_base + 0xF0);

    reg |= 0x80808080;

    writel_relaxed(reg, anatop_base + 0xF0);

    /* Make sure PLLs is disabled */

    reg = readl_relaxed(anatop_base + 0xA0);

    reg &= ~(1 << 13);

    writel_relaxed(reg, anatop_base + 0xA0);

    clk_data.clks = clk;

    clk_data.clk_num = ARRAY_SIZE(clk);

    of_clk_add_provider(np, of_clk_src_onecell_get, &clk_data);

    clk_register_clkdev(clk[gpt_ipg], "ipg", "imx-gpt.0");

    clk_register_clkdev(clk[gpt_ipg_per], "per", "imx-gpt.0");

    clk_register_clkdev(clk[gpt_3m], "gpt_3m", "imx-gpt.0");

    clk_register_clkdev(clk[cko1_sel], "cko1_sel", NULL);

    clk_register_clkdev(clk[ahb], "ahb", NULL);

    clk_register_clkdev(clk[cko1], "cko1", NULL);

    clk_register_clkdev(clk[arm], NULL, "cpu0");

    clk_register_clkdev(clk[pll4_audio_div], "pll4_audio_div", NULL);

    clk_register_clkdev(clk[pll4_sel], "pll4_sel", NULL);

    clk_register_clkdev(clk[lvds2_in], "lvds2_in", NULL);

    clk_register_clkdev(clk[esai], "esai", NULL);

    /*

     * The gpmi needs 100MHz frequency in the EDO/Sync mode,

     * We can not get the 100MHz from the pll2_pfd0_352m.

     * So choose pll2_pfd2_396m as enfc_sel's parent.

     */

    clk_set_parent(clk[enfc_sel], clk[pll2_pfd2_396m]);

    /* Set the parent clks of PCIe lvds1 and pcie_axi to be sata ref, axi */

    if (clk_set_parent(clk[lvds1_sel], clk[sata_ref]))

        pr_err("Failed to set PCIe bus parent clk.\n");

    if (clk_set_parent(clk[pcie_axi_sel], clk[axi]))

        pr_err("Failed to set PCIe parent clk.\n");

    /* gpu clock initilazation */

    clk_set_parent(clk[gpu3d_shader_sel], clk[pll2_pfd1_594m]);

    clk_set_rate(clk[gpu3d_shader], 594000000);

    clk_set_parent(clk[gpu3d_core_sel], clk[mmdc_ch0_axi]);

    clk_set_rate(clk[gpu3d_core], 528000000);

    clk_set_parent(clk[gpu2d_core_sel], clk[pll3_usb_otg]);

    for (i = 0; i < ARRAY_SIZE(clks_init_on); i++)

        clk_prepare_enable(clk[clks_init_on[i]]);

    if (IS_ENABLED(CONFIG_USB_MXS_PHY)) {

        clk_prepare_enable(clk[usbphy1_gate]);

        clk_prepare_enable(clk[usbphy2_gate]);

    }

    /* ipu clock initialization */

    init_ldb_clks(pll2_pfd0_352m);

    clk_set_parent(clk[ipu1_di0_pre_sel], clk[pll5_video_div]);

    clk_set_parent(clk[ipu1_di1_pre_sel], clk[pll5_video_div]);

    clk_set_parent(clk[ipu2_di0_pre_sel], clk[pll5_video_div]);

    clk_set_parent(clk[ipu2_di1_pre_sel], clk[pll5_video_div]);

    clk_set_parent(clk[ipu1_di0_sel], clk[ipu1_di0_pre]);

    clk_set_parent(clk[ipu1_di1_sel], clk[ipu1_di1_pre]);

    clk_set_parent(clk[ipu2_di0_sel], clk[ipu2_di0_pre]);

    clk_set_parent(clk[ipu2_di1_sel], clk[ipu2_di1_pre]);

    if (cpu_is_imx6dl()) {

        clk_set_rate(clk[pll3_pfd1_540m], 540000000);

        clk_set_parent(clk[ipu1_sel], clk[pll3_pfd1_540m]);

        clk_set_parent(clk[axi_sel], clk[pll3_pfd1_540m]);

        /* set epdc/pxp axi clock to 200Mhz */

        clk_set_parent(clk[ipu2_sel], clk[pll2_pfd2_396m]);

        clk_set_rate(clk[ipu2], 200000000);

    } else if (cpu_is_imx6q()) {

        clk_set_parent(clk[ipu1_sel], clk[mmdc_ch0_axi]);

        clk_set_parent(clk[ipu2_sel], clk[mmdc_ch0_axi]);

    }

    /*

     * Let's initially set up CLKO with OSC24M, since this configuration

     * is widely used by imx6q board designs to clock audio codec.

     */

    ret = clk_set_parent(clk[cko2_sel], clk[osc]);

    if (!ret)

        ret = clk_set_parent(clk[cko], clk[cko2]);

    if (ret)

        pr_warn("failed to set up CLKO: %d\n", ret);

    /* Audio clocks */

    clk_set_parent(clk[ssi1_sel], clk[pll4_audio_div]);

    clk_set_parent(clk[ssi2_sel], clk[pll4_audio_div]);

    clk_set_parent(clk[ssi3_sel], clk[pll4_audio_div]);

    clk_set_parent(clk[esai_sel], clk[pll4_audio_div]);

    clk_set_parent(clk[spdif_sel], clk[pll3_pfd3_454m]);

    clk_set_parent(clk[asrc_sel], clk[pll3_usb_otg]);

    clk_set_rate(clk[asrc_sel], 7500000);

    /* Set pll4_audio to a value that can derive 5K-88.2KHz and 8K-96KHz */

    clk_set_rate(clk[pll4_audio_div], 541900800);

    /* Set initial power mode */

    imx6_set_lpm(WAIT_CLOCKED);

    np = of_find_compatible_node(NULL, NULL, "fsl,imx6q-gpt");

    base = of_iomap(np, 0);

    WARN_ON(!base);

    irq = irq_of_parse_and_map(np, 0);

    mxc_timer_init(base, irq);

}

CLK_OF_DECLARE(imx6q, "fsl,imx6q-ccm", imx6q_clocks_init);

0 Kudos
3,957 Views
carlmichal
Contributor I

I'm looking at the patches to enable the higher VPU clock speed (looking to port to LK 3.14) and noticed something odd. One of the hunks in ENGR00317861 undoes one of the hunks in ENGR00313202

The last hunk in the first of those patches prevents the cpufreq device from being initialized and registered if CONFIG_ARM_IMX6_CPUFREQ is enabled, but this is reverted in the second patch.

Is that right?

nevermind - I should read the comment at the top of the patch.

0 Kudos
3,957 Views
carlmichal
Contributor I

Thanks! The source I was working from doesn't have this. I picked up

ENGR00320349, ENGR00317861, and ENGR00313202

and now in dmesg |grep VPU gives:

VPU 352M is enabled!

mxc_vpu 2040000.vpu: VPU initialized

remove 396MHz OPP for VPU running at 352MHz!

increase SOC/PU voltage for VPU352MHz

0 Kudos
3,957 Views
ralph__
Contributor IV

Hi, I tried googling for these hunks. Where do you get them from? Which repository?

Thanks,
Ralph

0 Kudos
3,957 Views
Tarek
Senior Contributor I

Thanks Yongcai,

Is there any known issues with this value?

I have enabled the configuration and it's working fine so far but I need to understand the side effects if any before we go to production.

Thanks

0 Kudos
3,957 Views
AnsonHuang
NXP Employee
NXP Employee

Hi,

     If enabling this config, the PLL2_PFD_400M will be set to 352M, as this PFD is also used by ARM for the lowest setpoint, so ARM freq of lowest setpoint will be lower from 400M to 352M.

     And, Higher VPU freq will need higher SOC/PU voltage, so the power consumption will be higher, I don't know how much, maybe you can measure it.

     Also, this PLL2_PFD_400M is used by busfreq driver for med setpoint of 400MHz DDR freq, now we didn't have this setpoint, but when we try this 352M VPU freq, we simply disable busfreq driver if this config is enabled. So, if you want BUS freq to work, you may need a small patch to enable it.

     There should be no significant side-effect for this config, but it may bring a little higher power consumption.

3,957 Views
Tarek
Senior Contributor I

Thanks again Yongcai,

I'm not worried about power consumption as the system is not running off battery. Also I'm fitting a heat sink and a fan for this product to be on the safe-side.

Thanks

0 Kudos
3,957 Views
AnsonHuang
NXP Employee
NXP Employee

OK, then there should be nothing to worry about as far as I know. You can do more stress test for your use case, good luck:)

0 Kudos