i.MX6Q FEC ethernet rate can't be up to 1000Mbit/sec, but only works with the 10/100Mbit.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q FEC ethernet rate can't be up to 1000Mbit/sec, but only works with the 10/100Mbit.

634 Views
nickruan
Contributor II

I test FEC ethernet rate with two MX6Q boards, the two boards are connected by 1000M  switcher. The board can only works with 10 or 100Mbit/sec rate, can't  transmit data with 1000Mbit/sec rate.

0 Kudos
Reply
1 Reply

519 Views
igorpadykov
NXP Employee
NXP Employee

Hi nick

please check signal timings with oscilloscope and

Table 62. RGMII Signal Switching Specifications i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

May be recommended to test with i.MX6Q Sabre SD reference board.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply