I test FEC ethernet rate with two MX6Q boards, the two boards are connected by 1000M switcher. The board can only works with 10 or 100Mbit/sec rate, can't transmit data with 1000Mbit/sec rate.
Hi nick
please check signal timings with oscilloscope and
Table 62. RGMII Signal Switching Specifications i.MX6DQ Datasheet (rev.4, 7/2015)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
May be recommended to test with i.MX6Q Sabre SD reference board.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------