i.MX6Q Ethernet Link silently down

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q Ethernet Link silently down

640件の閲覧回数
EinarMar
Contributor IV

I'm using kernel version 3.14.38 with rtpatch RT36 and am experiencing a link down from time to time. 

The problem is that there is no output from the kernel when it happens and to restore the link it's enough to replug the ethernet cable or restart the interface via ifconfig command. 

The device is connected to a 100Mbit switch if that is any hint !

I'd like to ask the community before commencing an ftrace search which can be time consuming.

regards

Einar

ラベル(3)
タグ(3)
0 件の賞賛
2 返答(返信)

521件の閲覧回数
b36401
NXP Employee
NXP Employee

Please check with ifconfig if "RUNNING" flag is missing at the moment the link is down. If so please check if the connection is OK.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

521件の閲覧回数
EinarMar
Contributor IV

The "RUNNING" flag is still present when the link is down. 

0 件の賞賛