i.MX6Q Ethernet Link silently down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q Ethernet Link silently down

653 Views
EinarMar
Contributor IV

I'm using kernel version 3.14.38 with rtpatch RT36 and am experiencing a link down from time to time. 

The problem is that there is no output from the kernel when it happens and to restore the link it's enough to replug the ethernet cable or restart the interface via ifconfig command. 

The device is connected to a 100Mbit switch if that is any hint !

I'd like to ask the community before commencing an ftrace search which can be time consuming.

regards

Einar

Labels (3)
0 Kudos
2 Replies

534 Views
b36401
NXP Employee
NXP Employee

Please check with ifconfig if "RUNNING" flag is missing at the moment the link is down. If so please check if the connection is OK.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

534 Views
EinarMar
Contributor IV

The "RUNNING" flag is still present when the link is down. 

0 Kudos