i.MX6Q: EIM_EB0,1 state at reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q: EIM_EB0,1 state at reset

Jump to solution
826 Views
norishinozaki
Contributor V

Hello Champs,

From Table 97 of DS, EIM_EB0,1 are Input for setting BOOT_CFG4.

pastedImage_2.png

pastedImage_3.png

From Table 100 of DS, the state of EIM_EB0,1 immediately after reset and before ROM firmware or software has executed, is Output.

Table100.png

From Table 101 of DS, "Before Reset State" of EIM_EB0,1 is Input.

pastedImage_13.png

If above all tables are correct, is this right understanding ?

EMI_EB0/1 are latched in BOOT_CFG4 in during the reset stage 1 below?

pastedImage_12.png

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
1 Solution
656 Views
art
NXP Employee
NXP Employee

Yes, your understanding is correct. The boot configuration signal inputs are latched at the time of the Reset signal de-assertion, and then they are immediately switched to their regular functionality.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
657 Views
art
NXP Employee
NXP Employee

Yes, your understanding is correct. The boot configuration signal inputs are latched at the time of the Reset signal de-assertion, and then they are immediately switched to their regular functionality.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
656 Views
norishinozaki
Contributor V

Thanks Artur!

Best regards,

Nori Shinozaki

0 Kudos
656 Views
BiyongSUN
NXP Employee
NXP Employee

Roughly. YES.

656 Views
norishinozaki
Contributor V

Thanks Biyong,

Have a good weekend!

Nori Shinozaki

0 Kudos