Hello Champs,
From AN4467 i.MX 6 Series DDR Calibration, DQM looks to be evaluated during calibration in 64 bit operation.
"associated DQS, DQM signals (as well as DDR clock). DDR_PHY1 delay and status registers are used for calibration of DQ[63:32] and associated DQS, DQM signals."
How about in 32-bit operations?
Is DQM used in Sabre SDP?
BR,
N.Shinozaki
解決済! 解決策の投稿を見る。
Hello,
For 32-bit DRAM I/F signals D32~D63, DQM4~7, and SDQS4~7 (_B)
are not used and can be left floating.
The SDP uses 64-bit memory I/F.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
For 32-bit DRAM I/F signals D32~D63, DQM4~7, and SDQS4~7 (_B)
are not used and can be left floating.
The SDP uses 64-bit memory I/F.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Yuri,
Thank you!
BR,
N.S.