Hello,
My customer is developing using i.MX6Q and BSP 3.10.17.
They would like to use LPCM in MPEG2-PS, and asking the spec such as bit rates, bit width and depth.
Are LPCM and MPEG2-PS supported in the BSP from the beginning?
As far as I checked, there is a table in i.MX_6_Series_Yocto_Project_Multimedia_Release_Notes.pdf.
I'm not sure this PCM means LPCM and the MPG2 includes Program Stream or not.
I also checked "audio/x-raw-int" fields by # gst-inspect in QSabreSD, however the results is not satisfaction.
# gst-inspect wavenc
SINK template: 'sink'
Availability: Always
Capabilities:
audio/x-raw-int
rate: [ 1, 2147483647 ]
channels: [ 1, 2 ]
endianness: 1234
width: 32
depth: 32
signed: true
audio/x-raw-int
rate: [ 1, 2147483647 ]
channels: [ 1, 2 ]
endianness: 1234
width: 24
depth: 24
signed: true
audio/x-raw-int
rate: [ 1, 2147483647 ]
channels: [ 1, 2 ]
endianness: 1234
width: 16
depth: 16
signed: true
audio/x-raw-int
rate: [ 1, 2147483647 ]
channels: [ 1, 2 ]
width: 8
depth: 8
signed: false
audio/x-raw-float
rate: [ 1, 2147483647 ]
channels: [ 1, 2 ]
endianness: 1234
width: { 32, 64 }
# gst-inspect wavparse
audio/x-raw-int
endianness: 1234
signed: { true, false }
width: { 8, 16, 24, 32 }
depth: [ 1, 32 ]
rate: [ 1000, 192000 ]
channels: [ 1, 8 ]
# gst-inspect auparse | more
SRC template: 'src'
Availability: Sometimes
Capabilities:
audio/x-raw-int
rate: [ 1, 2147483647 ]
channels: [ 1, 2147483647 ]
endianness: { 1234, 4321 }
width: { 8, 16, 24, 32 }
depth: [ 1, 32 ]
signed: { true, false }
audio/x-raw-float
rate: [ 1, 2147483647 ]
channels: [ 1, 2147483647 ]
endianness: { 1234, 4321 }
width: { 32, 64 }
# gst-inspect osssink
Pad Templates:
SINK template: 'sink'
Availability: Always
Capabilities:
audio/x-raw-int
endianness: { 1234 }
signed: { true, false }
width: 16
depth: 16
rate: [ 1, 2147483647 ]
channels: [ 1, 2 ]
audio/x-raw-int
signed: { true, false }
width: 8
depth: 8
rate: [ 1, 2147483647 ]
channels: [ 1, 2 ]
Best regards,
Nori Shinozaki
Have you tried the following command:
$ gst-inspect | grep imx
It should list the mpeg2 decoder:
mpeg2dec.imx: mfw_mpeg2decoder: mpeg2 video decoder
If not please make sure that the gstreamer package is selected on your image or add it on the local.conf file.
+ IMAGE_INSTALL_append=” packagegroup-fsl-gstreamer”
Hello, Thank you,
Yes, mpeg2dec is fine.
The trouble is demuxer(aiurdemux).
Please take a look at attached logs from gst-launch.
If LPCM format is S16BE, aiurdemux can demux video(MPEG2) and audio(LPCM) successfully.
However if it's S24BE, aiurdemux can't recognize the format type correctly.
The gst-launch log says "aiurdemux aiurdemux.c:3208:aiurdemux_parse_audio: Unknown Audio code-type=1, sub-type=8"
I checked sub-type=8 is defined as AUDIO_PCM_DVD in fsl_media_types.h
However in aiurdemux_parse_audio() in aiurdemux.c, AUDIO_PCM_DVD is not checked in case AUDIO_PCM sentence in line 3029.
Why is AUDIO_PCM_DVD not checked here?
How AUDIO_PCM_S24BE and AUDIO_PCM_DVD are distinguished?
Best regards,
Nori Shinozaki
Hello Champs,
Let me summerize this issue.
The customer would like to support a DVD format with gStreamer.
They are trying to re-use a FSL's aiurdemux plugin for the implementation.
The version is gst-fsl-plugins-3.0.7 in L3.0.35_4.1.0_130816.
However aiurdemux doesn't support some LPCM formats necessory for DVD, such as 20bit LPCM, big or little, signed or unsigned.
When we tried to look into the perser source, we found out the source code is not open.
It's a CORE_API (inf, getTrackType,,..). the implementation seems like Mpeg2GetTrackType in lib_mpg2_parser_arm11_elinux_hfp.so.3.1
Now we have come to a conclusion that there is one out of following solutions which the customer can take.
1. Freescale to modify aiurdemux to support full DVD format as the customer requests.
2. Freescale to disclose parser source code for the customer to modify by themselves.
3. Ask Richo to find other gStreamer demuxer plugin, if any.
4. Ask Richo to go to other multi-media middleware than gStreamer.
Could you please find any possibilities for #1 and 2?
Best regards,
Nori Shinozaki
I apologize. Unfortunately as mentioned on the note below table 3 of the Multimedia Release Notes, the demuxer support of a certain audio or video type does not necessarily mean that it can be played. This depends on the availability of the codec.
There was a known issue listed on previous releases of the BSP documentation where 24-bit PCM output was not supported by ALSALIB. In this scenario it would seems that the Linux Driver Audio might be part of the limitation as you mentioned.
The gstreamer source code is available on the BSP. You may find some more information on building gstreamer plugins on the following thread:
https://community.freescale.com/thread/300387
As for the possibility of Freescale to modify aiurdemux I would recommend consulting the Professional Engineering Services (link below)
http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL