Hello,
I want to drive 1920x720 @60hz LCD monitor with i.mx6q with my custom designed board. LCD requires typical 90 MHz LVDS DCLK.
I know i should use LDB in split mode. What confuses me is the clock frequency. Can i.mx6q drive 90 MHz LVDS clock for 2 channel LVDS at the resolution of 1920x720 @60hz?
Second question is that my LCD panel 2 channel LVDS interface, one channel for odd pixels and second channel for even pixels?
Do i have to connect the imx6 LVDS0 pins to odd channel of LCD and imx6 LVDS1 pins to even channel of LCD or vica versa?
Thanks..
Could you please verify that imx6q can drive 90 MHz clock on both LVDC0_CLK_P/N and LVDS1_CLK_P/N pads in split mode (both LVDS0 and LVDS1 signals are used)? This is a requirement for our LCD at 1920x720 @60 Hz.
The terminalogy in reference manuel really confuses me.
Could you verify this? Thanks
"LDB supports rates needed by WUXGA 16:10 aspect ratio (1920 x 1200 @
60 frames per second, data rate supported up to 170 MHz)."
from sect.39.4.1 Input Parallel Display Ports i.MX 6Dual/6Quad Applications Processor Reference Manual
Best regards
igor
Hello Igor,
Thanks for the reply.
"LDB supports rates needed by WUXGA 16:10 aspect ratio (1920 x 1200 @
60 frames per second, data rate supported up to 170 MHz)."
This sentence is unclear to me.
Is "up to 170 MHz clock" the lvds clock driven out of cpu? I need to give 90 MHz lvds clock signal to LCD.
Hi Mehmet
yes it can drive, frequency details can be found in sect.39.4.1 Input Parallel Display Ports
and connections in Table 39-5. Channel Mapping
i.MX 6Dual/6Quad Applications Processor Reference Manual
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thanks for the reply. I already checked the RM before opening this topic but i have unclear issues.
Table 39-5 mentions LVDS Channel 0 is mapped to DI0 first pixel, LVDS Channel 1 i mapped to DI0 second pixel.
What does it mean by first and second pixel? Does first pixel mean odd pixels, second pixel mean even pixels?