i.MX6Q 输出竖屏

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q 输出竖屏

1,221 Views
kaneshi
Contributor I

目前我司的i.MX6Q(QT5.6)的方案中使用的是4通道MIPI屏幕,是通过HDMI转MIPI DSI实现的。但是我们使用的是一个竖屏输出的MIPI屏幕,而i.MX6默认是横屏输出。我们想在kernel启动图标时进行竖屏输出,请问如何才能实现呢?

Labels (4)
0 Kudos
Reply
2 Replies

1,091 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Kane,

    我和I.MX Expert请教过这个问题,做旋转竖屏显示,必须要在应用层做,不能去修改显示驱动。而你要在kernel里把logo也竖起来,建议你在logo的作图上考虑一下,是不是把图竖起来。

-------------

I have ever asked i.mx expert on the question, Vertical display should be realized on application, you can't modify display driver. and if you want kernel logo to be vertical, you can consider it on drawing.

Have a nice day!

NXP TIC Weidong Sun

0 Kudos
Reply

1,091 Views
kaneshi
Contributor I

孙工你好,我们目前是这个情况。当前imx6如果跑1920.1080的横屏,此时如果采用指令方式以及开机logo为竖屏显示格式能够正常显示;但是选择的同样分辨率的竖屏1080.1920,则显示的是一半图像,不能平铺整个屏幕,无论怎么旋转。微信图片_20190108172926.jpg

0 Kudos
Reply