i.MX6DualLite : USB_H1_VBUS behavior on unpowered processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6DualLite : USB_H1_VBUS behavior on unpowered processor

跳至解决方案
1,716 次查看
koichisakagami
Contributor II

Dear community,

We are investigating the USB_H1_VBUS  behavior on custom board.

We know that
In i.MX6 USB VBUS can be powered any time,even to unpowered processor
from IMX6DLIEC sect.4.2.1 Power-Up Sequence.
USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and can be powered at any time.

[Background]
In the case of the i.MX6 powers off ,while the USB_OTG_VBUS is added with 5V,
the USB_H1_VBUS remains about 5 V.

When the i.MX6 powers off, on impressing a 5V to  the USB_OTG_VBUS,
the USB_H1_VBUS remains about 5 V.

Meantime,
in the case of  i.MX6 never power on ,
even if the USB_OTG_VBUS is added with 5V,
the USB_H1_VBUS does not appear 5 V.

[Question]
We think that this behavior is caused for the description in the datasheet IMX6SDLIEC 4.3.2.3 LDO_USB.
Is my understanding right ?

Best Regards,
Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,239 次查看
art
NXP Employee
NXP Employee

Yes, your understanding is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,240 次查看
art
NXP Employee
NXP Employee

Yes, your understanding is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,239 次查看
宗標廖
Contributor V

 

 

0 项奖励
回复