i.MX6Dual's system with battery.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Dual's system with battery.

ソリューションへジャンプ
1,176件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I'm considering i.MX6Dual's system with Li-ion battery.

Could you tell me how to detect the remaining battery level by i.MX6?

Best Regards,

Keita

ラベル(4)
0 件の賞賛
返信
1 解決策
1,096件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

one can add to design small adc with control over i2c/spi/uart or

use special devices lke below

Analog Devices Introduces Lithium-Ion Battery Monitoring and Protection System for Energy, Industria...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,097件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

one can add to design small adc with control over i2c/spi/uart or

use special devices lke below

Analog Devices Introduces Lithium-Ion Battery Monitoring and Protection System for Energy, Industria...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信