i.MX6Dual RTC_XTALI,RTC_XTALO pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6Dual RTC_XTALI,RTC_XTALO pins

跳至解决方案
1,855 次查看
佐藤智幸
Contributor I

Dear community,

I have a question about i.MX6Dual.

When I do not use external RTCXTAL(32.768k), is the RTC_XTALI,RTCXTALO pin good as a float?

Thanks and Best Regards,

标签 (1)
0 项奖励
回复
1 解答
1,610 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 佐藤智幸

you should always use RTCXTAL(32.768k) due to

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,611 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 佐藤智幸

you should always use RTCXTAL(32.768k) due to

ERR007926 ROM: 32 kHz internal oscillator timing inaccuracy may affect

SD/MMC, NAND, and OneNAND boot

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复