Hello community,
I have one question about Power-Down sequence for i.MX6DQP.
In Datasheet of i.MX 6DualPlus/6QuadPlus, IMX6DQPAEC rev 3, 11/2018,
Section 4.2.2 Power-Down Sequence say that
"There are no special restrictions for i.MX 6DualPlus/6QuadPlus SoC."
Is this applied only Supplies Contact in Table 95 ?
Or all contact both "Supplies Contact in Table 95." and "Functional Contact in Table 96." ?
Best regards,
Ishii.
Solved! Go to Solution.
Hello,
The power down requirements concern only power supply pins (mentioned in the Table 95).
All I/O pins must not be externally driven while the I/O power supply for the pin (NVCC_xxx)
is OFF. This can cause internal latch-up and malfunctions due to reverse current flows.
Regards,
Yuri.
Hello,
The power down requirements concern only power supply pins (mentioned in the Table 95).
All I/O pins must not be externally driven while the I/O power supply for the pin (NVCC_xxx)
is OFF. This can cause internal latch-up and malfunctions due to reverse current flows.
Regards,
Yuri.
Hello Yuri,
Thank you for your quick response.
Does it have some constraint between external drive off and I/O power supply off timing?
i.e. External driver must off faster than I/O power supply befor xx [ns].
Or is it OK to off at same time?
Best regards,
Ishii.
Hello,
Really there are no strict timing restrictions regarding external drive off and I/O
power supply off. So, the same time for the powers switching off is OK.
Regards,
Yuri.
Hello Yuri,
Thank you for your suggestion.
I will ask it to my customer.
Best regards,
Ishii.