i.MX6DQP Power-Down sequence.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQP Power-Down sequence.

Jump to solution
1,590 Views
takayuki_ishii
Contributor IV

Hello community,

I have one question about Power-Down sequence for i.MX6DQP.

In Datasheet of i.MX 6DualPlus/6QuadPlus, IMX6DQPAEC rev 3, 11/2018,

Section 4.2.2 Power-Down Sequence say that 

   "There are no special restrictions for i.MX 6DualPlus/6QuadPlus SoC."

Is this applied only Supplies Contact in Table 95 ?

Or all contact both "Supplies Contact in Table 95." and "Functional Contact in Table 96." ?

Best regards,

Ishii.

Labels (3)
Tags (1)
0 Kudos
Reply
1 Solution
1,489 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The power down requirements concern only power supply pins (mentioned in the Table 95).
All  I/O pins must not be externally driven while the I/O power supply for the pin (NVCC_xxx)

is OFF. This can cause internal latch-up and malfunctions due to reverse current flows.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
4 Replies
1,490 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The power down requirements concern only power supply pins (mentioned in the Table 95).
All  I/O pins must not be externally driven while the I/O power supply for the pin (NVCC_xxx)

is OFF. This can cause internal latch-up and malfunctions due to reverse current flows.

Regards,

Yuri.

0 Kudos
Reply
1,489 Views
takayuki_ishii
Contributor IV

Hello Yuri,

Thank you for your quick response.

Does it have some constraint between external drive off and I/O power supply off timing?

i.e. External driver must off faster than I/O power supply befor xx [ns].

Or is it OK to off at same time?

Best regards,

Ishii.

0 Kudos
Reply
1,490 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Really there are no strict timing restrictions regarding  external drive off and I/O

power supply off. So, the same time for the powers switching off is OK.

Regards,

Yuri.

0 Kudos
Reply
1,490 Views
takayuki_ishii
Contributor IV

Hello Yuri,

Thank you for your suggestion.

I will ask it to my customer.

Best regards,

Ishii.

0 Kudos
Reply