i.MX6DQ lifetime estimation out of range of AN4729.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ lifetime estimation out of range of AN4729.

654 Views
satoshishimoda
Senior Contributor I

Hi community,

Our patner have a question about i.MX6DQ life time estimation.

They want to esitmate the i.MX6DQ life time when they use i.MX6DQ under 85 degrees at Commercial 996MHz (1.225V) LDO enabled.
We can understand the lifetime is over 65,000 hours by AN4724, but cannot understand the concrete value since it is out of range.
Also, we don't estimate the lifetime when juction temperature < 100 degrees at industrial 792MHz (1.15V) LDO enabled.
So would you let me know how estimate the lifetime of the out of the figures in AN4724?

Then, I found i.MX6 product usage lifetime estimates , but not enough for them.
So would you give me the "lifetime calculator" if you can open it?

Best Regards,
Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

449 Views
Yuri
NXP Employee
NXP Employee

Hello,

  We do not provide "lifetime calculator"  tool. 

Customers can create requests for estimations.

Support|NXP 

Regards,

Yuri.

0 Kudos
Reply