i.MX6DQ NAND GPMI + BCH.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ NAND GPMI + BCH.

ソリューションへジャンプ
1,257件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

 

Our customer found a strange phenomenon with i.MX6DQ and SLC NAND.

They dumped same block of NAND with UBIFS.

Then, the data was not same between dumped with GPMI + BCH and dumped only with GPMI.

Please see the attached logs, you can see 0xF7 in line 89 of GPMI+BCH.txt.

Please give me advice why this difference was happen?

 

For your information, they got the dump data with gpmi_read_page function in gpmi driver (drivers/mtd/nand/gpmi-nand/gpmi-nand.c) in L3.0.101 BSP when mount ubifs partition for GPMI+BCH, and got with nanddump command (it seems to use gpmi_read_data function in gpmi driver) for GPMI only.

 

In fact, our customer's mass production has been stopped by related to this question.

So please give us your reply ASAP.

 

Best Regards,

Satoshi Shimoda

Original Attachment has been moved to: GPMI+BCH.txt.zip

Original Attachment has been moved to: GPMI.txt.zip

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 解決策
894件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  NAND is not reliable storage device. BCH is intended to correct possible errors.
It should be always used.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
895件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  NAND is not reliable storage device. BCH is intended to correct possible errors.
It should be always used.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信