Hi community,
I have a question about i.MX6SDL IPU CSI.
Please see the slide No. 56 of attached file in A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
It says the combining in the Image Conveter is upt to 40M pixels/sec with i.MX6DQ.
Next, please see chapter 37.1.2.1.5.3 in IMX6DQRM Rev.3, it says the IC perfomance is 200M pixels/sec for input and 100M pixels/sec for output.
To understand combining performance by Image Converter, which performance should I use?
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
Hi Satoshi
Image Conveter suppots many operations and RM gives max. IC perfomance.
IC combining performance is given in presentation.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
Image Conveter suppots many operations and RM gives max. IC perfomance.
IC combining performance is given in presentation.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------