i.MX6DQ DISP_CLK_PERIOD and DI_CLK_PERIOD.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ DISP_CLK_PERIOD and DI_CLK_PERIOD.

Jump to solution
670 Views
satoshishimoda
Senior Contributor I

Hi community,

I want to know how to calculate DISP_CLK_PERIOD and DI_CLK_PERIOD in datasheet (IMX6DQCEC Rev.4) chapter 4.11.10.6.3.

Datasheet says "The DISP_CLK_PERIOD, DI_CLK_PERIOD parameters are register-controlled.", so we can find dix_disp_clk_period in chapter 37.5.194 and chapter 37.5.230 in IMX6DQRM Rev.3.

Are these fields correspond with DISP_CLK_PERIOD?

And which register is correspond with DI_CLK_PERIOD?

Best Regards,

Satoshi Shimoda

Tags (2)
0 Kudos
Reply
1 Solution
541 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The sections 37.5.194 37.5.230 in IMX6DQRM about IPUx_DIy_BS_CLKGEN0

relate to DI_CLK_PERIOD, whereas DISP_CLK_DOWN and DISP_CLK_UP parameters
(which are set via the  Base Sync Clock Gen 1 Register) define DISP_CLK_PERIOD.

DISP_CLK_PERIOD may be considered as sum of DISP_CLK_DOWN and DISP_CLK_UP


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
542 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The sections 37.5.194 37.5.230 in IMX6DQRM about IPUx_DIy_BS_CLKGEN0

relate to DI_CLK_PERIOD, whereas DISP_CLK_DOWN and DISP_CLK_UP parameters
(which are set via the  Base Sync Clock Gen 1 Register) define DISP_CLK_PERIOD.

DISP_CLK_PERIOD may be considered as sum of DISP_CLK_DOWN and DISP_CLK_UP


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply