We are trying to support a new camera on CSI0 (parallel sensor interface). Our sensor works in ITU601 mode that looks like the "gated" mode, except that HSYNC is active during the complete duration of an image (starting 16 pixel clock cycles before the first HSYNC gets active, and stopping 16 pixel clock cycles after the last HSYNC gets inactive).
It doesn't match with the normal usage of the gated mode (described at §37.4.3.6.2 of the RM) but should work if the VSYNC is edge-triggered (either on the rising or the falling edge).
If the level of VSYNC is taken into account, it probably won't work.
Has anyone used gated mode with a similar signal VSYNC ?
Is there any internal information on GATED MODE indicating if such a VSYNC signal could also work ?
Thanks for any feedback.
已解决! 转到解答。
Hi Herve
you are right, VSYNC is edge-triggered and
this is mentioned in sect.4.11.10.2 Sensor Interface Timings
i.MX6DQ Datasheet (rev.4, 7/2015)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Herve
you are right, VSYNC is edge-triggered and
this is mentioned in sect.4.11.10.2 Sensor Interface Timings
i.MX6DQ Datasheet (rev.4, 7/2015)
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
OK, VSYNC is latched on the rising edge when working in GATED MODE.
§4.11.10.2.2 of http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf seems wrong concerning data sampling : "Data is latched at the rising edge of the valid pixel clocks." Chronogramms clearly show that data sampling occur on the falling edge of the pixel clock.
What are the blanking constraints when working in GATED MODE ?
I didn't find information on this topic in the manuals... To be more precise, this question could be split in several sub-questions :
For information, here is a capture of our VSYNC rising edge followed by HSYNC assertion. Signals are a bit noisy due to cables soldered on our PCB. Is there anything wrong explaining why it doesn't work (320x200 in YUV422) ?
one can look at docx on link below
About HSYNC timing of CSI input in i.MX6DQ.
also had you set correct CSI_DATA_EN as described below
~igor