i.MX6DL vs. i.MX6DP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL vs. i.MX6DP

1,066 Views
PaulDeMetrotion
Senior Contributor I

We are developing a device that supports the i.MX6DL and i.MX6DP processors. Is there a separate device tree for the DP processor? If so, what is it called?

0 Kudos
Reply
1 Reply

832 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paul

I am afraid there is no separate device tree for the DP, and QP dts may be used:

arch/arm/boot/dts/imx6qp-sabresd.dts

linux-imx.git - i.MX Linux Kernel 

As example of D device tree one can check SCM-i.MX6D: Single Chip Module-i.MX6D (compare it with

corresponding SCM-i.MX6Q)
https://www.nxp.com/products/single-chip-modules/single-chip-module-i.mx-6d:SCM-i.MX6D?tab=Design_To...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply