i.MX6DL: USB Transmitter/Reciver Control Register setting in IBIS model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL: USB Transmitter/Reciver Control Register setting in IBIS model

Jump to solution
998 Views
kazuoasano
Contributor II

Hi community,

We are simulating by the following IBIS file.

  i.MX 6DualLIte and i.MX 6Solo IBIS File(REV 1.4.)

Finally, We would like to confirm the signal difference by a simulation and our circuit board.

Therefore, I want to know register setting of IBIS model.

In addition information, A reference manual is described as follows.
"66.2.6 Recommended Register Configuration for USB Certification"

  See : i.MX 6Solo/6DualLite Applications Processor Reference Manual (REV 2)   P.5537

This is different from register setting of default.

   See : i.MX 6Solo/6DualLite Applications Processor Reference Manual (REV 2)   P.5545

             66.3.2 USB PHY Transmitter Control Register (USBPHYx_TXn)

Register field parameterRecommend for USB CertificationDefault value
HW_USBPHY_TX_TXCAL45DP0x00x6
HW_USBPHY_TX_TXCAL45DN0x00x6
HW_USBPHY_TX_D_CAL0x70x7

  

What kind of a register setting in IBIS model is it?

Labels (2)
1 Solution
720 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kazuo,

According with AE team, configuration options on USB IBIS are not provided. It is preferred to tune the registers during USB compliance test, as simulation can't replace compliance test.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
720 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kazuo,

We have internally escalated your request, you will receive additional details soon.

Best regards!

/Carlos

720 Views
kazuoasano
Contributor II

Hi Carlos,

Thank you for response.


Please teach Detail USB register setting.
In addition, If possible, Please teach me the iomux setting on IBIS model in completely all function.

/Kazuo

0 Kudos
721 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kazuo,

According with AE team, configuration options on USB IBIS are not provided. It is preferred to tune the registers during USB compliance test, as simulation can't replace compliance test.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
720 Views
kazuoasano
Contributor II

> configuration options on USB IBIS are not provided.
I can't understand why couldn't be provided a configuration options on USB IBIS.

So, There is no help for it...

We don't never think that simulation can't replace compliance test.
Only,I just want to confirm the signal difference by a simulation design of IBIS and our circuit board.


I am extremely disappointed.

thanks,

/Kazuo

0 Kudos