Hi
I bought an Congatec module i.MX6DL/Solo-QMX6 but when I use MfgTool to create the SD card it doesn't work. It works fine until "Jumping to OS image" but then it fails with following error messages:
1 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="900" onError="" text="" FAIL code=0xffff0002.
Panel A: Wrong device found.,failed to run command: type="find" body="Updater" file="" timeout="900" onError="" text=""
2 - Panel A Finished processing QMX6 usdcard-partition-install <LIST/> : FAIL code=-65534.
Does anyone knows how I can solve this problem?
Because the MfgTool doesn't work, I also created an µSD card using cfImager.exe, but I don't manage to boot E-Boot. It's quite weird because I already did those things succesfully for the Imx53QSB, and there everything works fine if you create a µSD card with cfImager.exe, it Boots immediately.
Do I have to set additional settings in U-Boot, or how can I define the correct address in the environment variables of U-boot? Now I tried several things, such as
mmc dev 0; mmc read ${loadaddr} 0x800 0x2000; bootm
But this doesn't work.
Can anyone help me on this topic? Or does someone has binaries that work fine for this module?
Kind regards
Nele Perdu
MFGTool has only been tested with Freescale's own evaluation boards, we don't know if it would work to flash a Congatec with Windows CE7.
Hi Nele,
I am so sorry that we don't have WinCE BSP for i.MX6. But our third party provide the WinCE BSP for i.MX6, this mean that you could connect the third party .
Hope this can help you ~~
Best Regards
Dan