I just received an i.MX6DL SABRE platform. The Android ICS image that was preloaded on the provided SD card booted successfully, but now I'm having trouble updating the platform to the most recent prebuilt Android image provided by Freescale. So far, I've followed the provided Android Quick Start Guide step by step:
Here's where I'm encountering the problem.
When I try to run the MFGTool, a window comes up saying "Can't find the specified file." Below is the resulting LOG file:
DLL version: 2.1.1
Tuesday, July 23, 2013 10:20:54 Start new logging
ModuleID[1] LevelID[10]: Parse C:\Users\moonej\Sabre Platform 2\Mfgtools-Rel-4.0.0_130424_MX6DL_UPDATER\cfg.ini file success[chip: MX6DL Linux Update, List: Android-SABRESD-eMMC]
ModuleID[2] LevelID[1]: Boot command-- file C:\Users\moonej\Sabre Platform 2\Mfgtools-Rel-4.0.0_130424_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\u-boot.bin failed to open.errcode is 2
ModuleID[1] LevelID[1]: Parse C:\Users\moonej\Sabre Platform 2\Mfgtools-Rel-4.0.0_130424_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\ucl2.xml failed
Can someone help me out with this?
已解决! 转到解答。
The problem is fixed.
The changes to the xml file mentioned above were correct except for the second change. That line should read <CMD state="Updater" type="push" body="send" file="files/android/u-boot-mx6dl-sabresd.bin">Sending U-Boot</CMD> like it originally stated. Changing the u-boot file name and the mmcblk were the missing pieces.
Thanks for your help
Thanks for your reply.
I made the change you suggested as well as a few others. After looking at the xml file, I realized there is no profile called "Android-SabreSD-SD". Another thread suggested to use the "Android-SabreSD-eMMC" profile but change the "mmcblk0" to "mmcblk1" in order to write to the SD card.
I also changed the xml from <CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot-mx6dl-sabresd.bin" >Loading U-boot</CMD "
to <CMD state="BootStrap" type="boot" body="BootStrap" file ="u-boot.bin" >Loading U-boot</CMD
And I changed the xml one more time from
| <CMD state="Updater" type="push" body="send" file="files/android/u-boot-mx6dl-sabresd.bin">Sending U-Boot</CMD> |
to
| <CMD state="Updater" type="push" body="send" file="files/android/u-boot.bin">Sending U-Boot</CMD> |
With these changes the MFGTool runs, but it hangs at "Loading U-boot." Any suggestions?