i.MX6DL GPU graphic library performance.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL GPU graphic library performance.

Jump to solution
1,030 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner will use i.MX6DL GPU for graphic operation with L3.0.35_4.1.0.

Then, they want to use a graphic library which has best performance.

Could you let me know which graphic library has best performance for the following functions?

(e.g. draw a line => DirectFB 2D acceleration library, alfa blending => OpenVG 1.1 library, etc...)

[Main functions]

Draw a line

Fill a picture with a color of user choice

Put a bitmap image

Use alfa blending

*3D graphic is not used.

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (1)
0 Kudos
1 Solution
741 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

i do not think that we have such performance characteristics.

Best regards

chip

View solution in original post

0 Kudos
3 Replies
741 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi, please look at FTF WorkShop

"Introduction to OpenVG", it gives good examples of graphic libraries usage

http://cache.freescale.com/files/training/doc/ftf/2014/FTF-AUT-F0342.pdf

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

741 Views
satoshishimoda
Senior Contributor I

Hi chipexpert,

I checked the document, it is useful if we use OvenVG.

But I felt it does not mentioned about performance, doesn't it?

Could you give me advice what library has best performance to our functions?

Best Regards,

Satoshi Shimoda

0 Kudos
742 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

i do not think that we have such performance characteristics.

Best regards

chip

0 Kudos