i.MX6DL, Dora, Kernel 3.10.17: PCIe Bridge Support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DL, Dora, Kernel 3.10.17: PCIe Bridge Support?

1,406 Views
leoschwab
Contributor III

So it looks like kernel 3.10.9_alpha doesn't do PCIe so well.  Transitioning to kernel 3.10.17_beta allowed the system to come up and see the PCIe bus, but all it's seeing is our bridge chip:

PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x1000-0x10000]

pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]

pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]

PCI: bus0: Fast back to back transfers disabled

PCI: bus1: Fast back to back transfers enabled

pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]

pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]

pci 0000:00:00.0: PCI bridge to [bus 01]

We had PCIe bridging working in 3.0.35, but we had to apply a kernel patch to get it to work.  Is a patch also required for the 3.10.x series kernels?

Schwab

Labels (2)
0 Kudos
Reply
2 Replies

878 Views
leoschwab
Contributor III

For those playing at home:  After a bunch of Google searches and reading a few dozen messages on the linux-arm-kernel mailing list, it appears that PCIe bus support is still very active for i.MX6, and that anyone playing there should expect a bumpy ride.

Applying the patch series beginning here (with some hand-tuning) allowed us to enumerate the devices plugged into the PCIe switch:

[PATCH 1/7] PCI: imx6: Make reset-gpio optional

Schwab

878 Views
sinanakman
Senior Contributor III

Hi Leo, I wonder which board you are using and also what is your pcie device. I am taking up on some pcie work with sabresd and an xhci based board so I'd like to know where you stand with your experiences so far. Are you using latest mainline kernel ?

Thanks

Sinan Akman

0 Kudos
Reply