i.MX6DL - Determine Boot From Recovery Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DL - Determine Boot From Recovery Device

ソリューションへジャンプ
2,653件の閲覧回数
christian_neuwi
Contributor III

Hi,

we're building our own hardware based on an i.MX6DL using an eMMC as primary boot device and an SPI NOR Flash as recovery device.

Our board behaves as expected when there is no bootloader in eMMC, i.e. it boots from SPI NOR Flash, but I can find no indication about that fact in any of the SRC registers I've been looking at.

Is there such an indication at all and - if so - where can I find it?

Regards,

Chris.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,458件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chris

I am afraid there is no such indication which recovery device was used.

Best regards igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,458件の閲覧回数
christian_neuwi
Contributor III

FYI:

The flag PERSIST_SECONDARY_BOOT (SRC_GPR10[30]) does indicate that booting occurred from the recovery device. It might not say exactly which recovery device was used, but since you can have only one that information is usually good enough for the firmware to react appropriately if needed.

Best regards,

Chris.

0 件の賞賛
返信
2,459件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chris

I am afraid there is no such indication which recovery device was used.

Best regards igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信