Hi All,
I'm implementing the DTS file for the Utilite standard board. The kernel is booting but not mounting the rootfs from SDcard.
Looks like the MMC is not configured correctly. The mmc driver keeps rescanning with different frequencies forever!
How do I configure it correctly?
Attached the dts files.
Kernel log:
U-Boot 2009.08-cm-fx6-0.91+tools (Nov 19 2013 - 14:56:48)
CPU: Freescale i.MX6 family TO6.4 at 792 MHz
Temperature: 34 C, calibration data 0x56b4dd69
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 29333333Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 11000000Hz
Board: CM-FX6:[ WDOG ]
Boot Device: SD
I2C: ready
RAM Configuration:
Bank #0: 10000000 1 GB
Bank #1: 80000000 1 GB
NAND: No NAND device found!!!
0 MiB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2
JEDEC ID: 0x20:0x71:0x15
In: serial
Out: serial
Err: serial
Net: got MAC address from IIM: 00:00:00:00:00:00
FEC0
Hit any key to stop autoboot: 3 2 1 0
mmc2 is current device
Loading file "boot/uImage" from mmc device 2:1 (xxc1)
5212512 bytes read
## Booting kernel from Legacy Image at 10800000 ...
Image Name: Poky (Yocto Project Reference Di
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5212448 Bytes = 5 MB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.10.17-1.0.0_beta+gec1af9f (telsherbiny@HP-Elite7500) (gcc version 4.8.1 (GCC) ) #6 SMP Fri Feb 14 16:23:21 GMT 2014
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: ADH i.MX6 Dual utilite Board from compu-lab
Ignoring RAM at 80000000-bfffffff (vmalloc region overlap).
cma: CMA: reserved 256 MiB at 40000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @81983000 s8704 r8192 d15872 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc3,115200 video=mxcfb0:dev=hdmi,1920x1080@60 fbmem=24M,10M root=/dev/mmcblk0p1 rw rootwait rootfs=ext3 enable_wait_mode=off consoleblank=0 video=mxcfb1:off video=mxcfb2:off video=mxcfb2:off maxcpus=2
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1024MB = 1024MB total
Memory: 763580k/763580k available, 284996k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
modules : 0x7f000000 - 0x80000000 ( 16 MB)
.text : 0x80008000 - 0x80bdb58c (12110 kB)
.init : 0x80bdc000 - 0x80c26200 ( 297 kB)
.data : 0x80c28000 - 0x80c76320 ( 313 kB)
.bss : 0x80c76320 - 0x80cdabe4 ( 403 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6Q, silicon rev 1.2
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x806173a0 - 0x806173f8
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (3162.11 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
init imx6q_init_machine
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1125 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2425 mV
cpu: 725 <--> 1450 mV at 1150 mV
vddpu: 725 <--> 1450 mV at 1150 mV
vddsoc: 725 <--> 1450 mV at 1200 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
2P5V: 2500 mV
3P3V: 3300 mV
usb_otg_vbus: 5000 mV
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
cfg80211: Calling CRDA to update world regulatory domain
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
pureg-dummy: no parameters
imx6_busfreq busfreq.13: DDR medium rate not supported.
Bus freq driver module loaded
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 2003
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
MIPI DSI driver module loaded
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 1.1
imx-sdma 20ec000.sdma: initialized
Serial: IMX driver
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
console [ttymxc3] enabled
serial: Freescale lpuart driver
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
ahci: SSS flag set, parallel bus scan disabled
ahci ahci: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
m25p80 spi32766.0: found mr25h256, expected sst25vf016b
m25p80 spi32766.0: mr25h256 (32 Kbytes)
spi_imx 2008000.ecspi: probed
CAN device driver interface
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver usb-storage
imx_usb 2184000.usb: usbmisc init failed, ret=-517
platform 2184000.usb: Driver imx_usb requests probe deferral
imx_usb 2184200.usb: usbmisc init failed, ret=-517
platform 2184200.usb: Driver imx_usb requests probe deferral
mousedev: PS/2 mouse device common for all mice
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode
mmc0: no vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode
mmc1: no vqmmc regulator found
mmc1: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
ata1: SATA link down (SStatus 0 SControl 300)
Galcore version 4.6.9.9754
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
caam 2100000.caam: device ID = 0x0a16010000000000 (Era -524)
caam 2100000.caam: job rings = 2, qi = 0
caam 2100000.caam: authenc-hmac-md5-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-md5-cbc-aes-caam
caam 2100000.caam: authenc-hmac-sha1-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-sha1-cbc-aes-caam
caam 2100000.caam: authenc-hmac-sha224-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-sha224-cbc-aes-caam
caam 2100000.caam: authenc-hmac-sha256-cbc-aes-caam
caam 2100000.caam: authencesn-hmac-sha256-cbc-aes-caam
caam 2100000.caam: authenc-hmac-md5-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-md5-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-sha1-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-sha1-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-sha224-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-sha224-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-sha256-cbc-des3_ede-caam
caam 2100000.caam: authencesn-hmac-sha256-cbc-des3_ede-caam
caam 2100000.caam: authenc-hmac-md5-cbc-des-caam
caam 2100000.caam: authencesn-hmac-md5-cbc-des-caam
caam 2100000.caam: authenc-hmac-sha1-cbc-des-caam
caam 2100000.caam: authencesn-hmac-sha1-cbc-des-caam
caam 2100000.caam: authenc-hmac-sha224-cbc-des-caam
caam 2100000.caam: authencesn-hmac-sha224-cbc-des-caam
caam 2100000.caam: authenc-hmac-sha256-cbc-des-caam
caam 2100000.caam: authencesn-hmac-sha256-cbc-des-caam
caam 2100000.caam: ecb-des-caam
caam 2100000.caam: ecb-arc4-caam
caam 2100000.caam: ecb-aes-caam
caam 2100000.caam: ctr-aes-caam
caam 2100000.caam: cbc-aes-caam
caam 2100000.caam: ecb-des3-caam
caam 2100000.caam: cbc-3des-caam
caam 2100000.caam: cbc-des-caam
caam 2100000.caam: fsl,sec-v4.0 algorithms registered in /proc/crypto
platform 2101000.jr0: registering rng-caam
platform caam_sm: caam_sm_test: 8-byte key test match OK
platform caam_sm: caam_sm_test: 16-byte key test match OK
platform caam_sm: caam_sm_test: 32-byte key test match OK
platform caam_secvio.19: security violation service handlers armed
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
sgtl5000 0-000a: Failed to get supply 'VDDD': -19
0-000a: 1200 mV normal
sgtl5000 0-000a: Using internal LDO instead of VDDD
sgtl5000 0-000a: Device with ID register ffff is not a sgtl5000
sgtl5000 0-000a: ASoC: failed to probe CODEC -19
imx-sgtl5000 sound.18: ASoC: failed to instantiate card -19
imx-sgtl5000 sound.18: snd_soc_register_card failed (-19)
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
ALSA device list:
No soundcards found.
Waiting for root device /dev/mmcblk0p1...
mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz
mmc0: mmc_rescan_try_freq: trying to init card at 300000 Hz
mmc0: mmc_rescan_try_freq: trying to init card at 200000 Hz
mmc0: mmc_rescan_try_freq: trying to init card at 100000 Hz
mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz
mmc0: mmc_rescan_try_freq: trying to init card at 300000 Hz
............
........... FOREVER
Original Attachment has been moved to: imx6d-utilite-std.dtb.zip
Original Attachment has been moved to: imx6d.dtsi.zip
Solved! Go to Solution.
The Card Detection pin is not working. I've disabled the configuration in DTS file:
&usdhc3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc3_2>;
// cd-gpios = <&gpio7 1 0>;
// wp-gpios = <&gpio7 0 0>;
vmmc-supply = <®_3p3v>;
status = "okay";
};
The rootfs is now mounting! I will look into the CD pin later when everything else is working.
Thanks guys for trying to help
The Card Detection pin is not working. I've disabled the configuration in DTS file:
&usdhc3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc3_2>;
// cd-gpios = <&gpio7 1 0>;
// wp-gpios = <&gpio7 0 0>;
vmmc-supply = <®_3p3v>;
status = "okay";
};
The rootfs is now mounting! I will look into the CD pin later when everything else is working.
Thanks guys for trying to help
It looks like you have two mmc devices (mmc0, mmc1) - are you sure you're trying to mount rootfs from the correct one? Currently it's /dev/mmcblk0p1 . u-boot says:
> Loading file "boot/uImage" from mmc device 2:1 (xxc1)
which makes me think maybe you want mmcblk1p1...
Hi Kursad,
The boot device might not be configured correctly in u-boot but I don't think this is the problem.
If the SD card was detected correctly I should see something like:
mmc1: new high speed SDHC card at address aaaa
Also the Kernel should tell me the device name like this message :
mmcblk0: mmc1:aaaa SU08G 7.40 GiB
But that's not the case. I think the kernel is not detecting the card for some reason but I don't know why?
I doubt that upgrading U-boot will solve the problem because U-boot can read the uImage from the SD card and boot the kernel. Then the kernel after several initializations waits for the rootfs device to show up as if the card was not present!
Anyway I will try to get a more recent u-boot and see if that helps.
Thanks,
Tarek
Why are you using U-Boot 2009.08-cm-fx6-0.91+tools (Nov 19 2013 - 14:56:48)?
Hi Daiane,
I don't have the latest U-boot for this board. What can I do ....... :smileysad:
But it seams that combining the dtb file with uImage is working. As you can see U-boot is booting the image. Do you think that's wrong?
:smileysad:
as I remeber, imx6 development over u-boot 2009.08 stoped 6/8 months ago
Now, any development as been making on u-boot 2013.04
If you're using your custom board, you should be using your custom kernel. So, maybe you could only verify latest patches from FSL regarding voltage/pmic changes.
I would say it's probably you're facing a u-boot X kernel mismatch