i.MX6D USB operation voltage PMU_REG_3P0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6D USB operation voltage PMU_REG_3P0

400 Views
sugiyamatoshihi
Contributor V

Hi,

Regarding to USB regulator output voltage, it is set 3.2V by OUTPUT_TRG in  PMU_REG_3P0 register.

I think USB normally use 3.3V.  Also, uboot use default value of 3.0V.

Are there any reason to set the voltage as 3.2V in Linux?

Best Regards,

Sugiyama

Labels (3)
0 Kudos
1 Reply

287 Views
art
NXP Employee
NXP Employee

There is no special reason to set 3.2V output. All voltages in range of 3.0V to 3.3V are valid for USB operation.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos