i.MX6D - DDR差分时钟终端电阻

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6D - DDR差分时钟终端电阻

2,208 Views
jcteng
Contributor I

         在i.MX6D的参考设计中,DDR的差分时钟要求要有终端电阻200Ω,如图片中R118和R43。请问这个终端电阻的作用是什么?如果不加这个终端电阻,可能会有什么风险?谢谢!

TIM截图20200103134021.jpg

Labels (2)
0 Kudos
Reply
1 Reply

2,083 Views
igorpadykov
NXP Employee
NXP Employee

Hi jcteng

these resistors are used for decreasing signal reflections and improving

signal shape.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply