I am trying to load u-boot onto an i.MX6DL board via JTAG without using any other peripherals (ie, USB, SD card, etc). I am using an ARM DSTREAM JTAG debugger.
In the past, I was able to do this with u-boot 2009.08 using the u-boot elf file. I would do the following:
1. Connect to board with JTAG
2. Load DDR .ds script to initialize DDR registers
3. Load the u-boot ELF file
4. Start the debugger
5. Board would boot that loaded u-boot out of memory.
However, when I try with the current version of u-boot 2016.03, DSTREAM won't even load the u-boot elf file properly. Something has changed in u-boot since 2009 and they use some ELF headers that prevents debuggers from loading the ELF file properly. So now I am trying to use the "restore" command in DSTREAM to load u-boot. The procedure I'm tying is:
1. Connect to board with JTAG
2. Load DDR .ds script to initialize DDR registers
3. Execute the following commands on debugger to load u-boot:
# disable IRQs, MMU and cache
set var $Core::$CPSR.I = 0x1
set var $Core::$CPSR.F = 0x1
set var $CP15::$SBanked::$S_SCTLR.M = 0
set var $CP15::$SBanked::$S_SCTLR.C = 0
# Load binary into memory
restore u-boot.bin binary 0x17800000
# load symbols
add-symbol-file u-boot SP:0x0
# set PC
set var $PC = 0x17800000
set debug-from *0x17800000
4. Start the debugger
5. u-boot does not start
I'm assuming NXP uses DSTREAM debuggers to do this, so if anyone can point out what I'm doing wrong I would appreciate it.
已解决! 转到解答。
Hello,
You may look at the following Community post :
How to Use Trace32 to Run U-boot in the i.MX6Q SABRE Platform
Also, I sent You document ; hope it helps.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct
Answer button. Thank you!