i.MX6 specific registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 specific registers

Jump to solution
1,243 Views
aditkous
Contributor I

Hello,

I was going through the reference manual to get the base addresses and size of the following. Been unsuccessful so far. Could someone fill me in?

MMIO_BASE, MMIO_SIZE, IIM_BASE, IIM_SIZE, TZIC_BASE, TZIC_SIZE, CACHE_LINE_SIZE_LOG2.

Plus, there is a MPR121.h (which is a capacitive touch processor) for i.MX53. Is there an i.MX6 equivalent?

Thanks and regards,

Aditya

PS. If one is able to get these values, can it be appended by the source?

Labels (6)
0 Kudos
Reply
1 Solution
752 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Aditya

     What is MMIO module?

     IIM_BASE now called OCOTP, its address is 0x21bc000, for iMX6, there is no TZIC, now use common interrupt controller called GIC, this is ARM standard interrupt controller. What is CACHE_LINE_SIZE_LOG2? The cache line size is 32 bytes.

View solution in original post

0 Kudos
Reply
1 Reply
753 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Aditya

     What is MMIO module?

     IIM_BASE now called OCOTP, its address is 0x21bc000, for iMX6, there is no TZIC, now use common interrupt controller called GIC, this is ARM standard interrupt controller. What is CACHE_LINE_SIZE_LOG2? The cache line size is 32 bytes.

0 Kudos
Reply