i.MX6 solo latest BSP and linux version support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 solo latest BSP and linux version support

Jump to solution
458 Views
hitesh_gambhava
Contributor I

Hi NXP team,

I was checking on i.MX6 solo design resourcing and found that they have mentioned Linux version 3.10 only.

My question is can i.MX6 solo support latest Linux kernel version? If not, what is the maximum kernel version supported over this processor?

We are workign on one product optimization which was build with Linux kernel version 3.10.

Looking forward to your response.

Thanks,

Hitesh

Labels (2)
0 Kudos
Reply
1 Solution
433 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava 

If you are mentioning the i.MX6 solo, then we can see it supported as the latest version from the link Embedded Linux for i.MX Applications Processors | NXP Semiconductors

 

Regards

Harvey

View solution in original post

0 Kudos
Reply
2 Replies
434 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava 

If you are mentioning the i.MX6 solo, then we can see it supported as the latest version from the link Embedded Linux for i.MX Applications Processors | NXP Semiconductors

 

Regards

Harvey

0 Kudos
Reply
414 Views
hitesh_gambhava
Contributor I

Thanks Harvey.

Best regards,

Hitesh

0 Kudos
Reply