i.MX6 solo dual display wayland

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 solo dual display wayland

Jump to solution
1,594 Views
swid
Contributor I

We have run dual-display wayland (LVDS + HDMI) on an i.MX6q SabreSD with a GC2000.

Could that setup be run on an i.MX6 solo with a GC880?

Will we be able to run egl applications on both displays?

Labels (3)
0 Kudos
1 Solution
798 Views
igorpadykov
NXP Employee
NXP Employee

yes, it is accelerated.

View solution in original post

0 Kudos
3 Replies
798 Views
igorpadykov
NXP Employee
NXP Employee

Hi swid

supported only GC2000 and GC320 as described in attached document

sect.15.5.1 Multi display support..

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
798 Views
swid
Contributor I

Ok, as the i.MX6 solo has a GC320 we will be able to use dual display, egl accelerated wayland on a i.MX6 solo based system?

0 Kudos
799 Views
igorpadykov
NXP Employee
NXP Employee

yes, it is accelerated.

0 Kudos