i.MX6 solo MIPI DSI 2 lanes支持的最高分辨率是多少?能否支持720x1280

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 solo MIPI DSI 2 lanes支持的最高分辨率是多少?能否支持720x1280

3,423 Views
yongheluo_hotma
Contributor III

Dear Sir,

     敝司有一个新项目,LCD屏为:720x1280的MIPI接口(驱动IC为:st7703),需要用到i.MX6 Solo MIPI_DSI接口去驱动这个LCD屏。

    在《i.MX 6Solo/6DualLite Applications Processor Reference Manual》第42.2章节(如图1),写到“Programmable display resolutions, from 160x120(QQVGA) to 1280x720(XVGA).”

    在 《i.MX 6 Linux Reference Manual》第7.1.1章节(如图2),写到“Programmable display resolutions, from 160x120(QQVGA) to 1024x768(XVGA)”

    到底哪个信息是正确的?

    敝司经过很长时间的调试,虽然LCD能够被点亮,但是会出现拖影,长时间运行后会出现残影等各种问题。尝试修改各种参数(如:colck、H/VBP等),均不能达到预期的效果。

    故需要跟贵司确认一下:

         i.MX6 solo MIPI DSI 2 lanes支持的最高分辨率是多少?能否支持720x180吗?

    另外,i.mx6平台一次只能发送64个字节的MIPI命令(含DCS type),我们所使用的LCD初始化命令中,有一条刚好超出这个范围(一个cmd + 63个参数)。因此,平台是否能够发送超出64个字节的命令呢?

image003.jpg

image004.jpg

    谢谢!

    罗永和

0 Kudos
3 Replies

2,932 Views
igorpadykov
NXP Employee
NXP Employee

Hi yonghe

correct is sect.42.2 Features i.MX6SDL Reference Manual: "1280x720".

For supported commands one can look at Table 42-2. DSI packet types for DCS commands

i.MX 6Solo/6DualLite Applications Processor Reference Manual

Also may be useful to check erratum ERR005191 MIPI: Corruption of short command

Chip Errata for the i.MX 6Solo/6DualLite

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,932 Views
yongheluo_hotma
Contributor III

Dear Igor,

    非常感谢您的回复。

    我们目前用的LCD模组的分辨率为:720x1280; driver IC为:st7703.

    虽然LCD能点亮和显示,但是会出现残影和拖影的情况,如图1。实际上的显示原图为图2.(即:在图1中产生了拖影)

图1

   微信图片_20190724114820.jpg

-------------------------------------------

图2:

test_picture.bmp

    如果采样另外一块模组(1024x600),则不会存在这一问题。

    尝试调试各种参数都没有办法解决。

    所以,需要您帮忙提供一些调试的思路,如:调整哪些参数(尤其是clock等timing)也许可能解决这一问题?

    谢谢!

    罗永和

0 Kudos

2,932 Views
yongheluo_hotma
Contributor III

Dear Igor,

     该问题已经解决,可能跟LCD的AVDD的电压和个别LCD的参数有关。

     谢谢!

     罗永和

0 Kudos